Structure containing the min and max values for a given PA and voltage supply combination (in deci-dBm).

Public Attributes#

int16_t

max deci-dBm value

int16_t

min deci-dBm value

Pointer to "piecewiseSegments"-length array of RAIL_TxPowerCurveSegment_t of power (deci-dBm) to powerLevel conversion fits.

Public Attribute Documentation#

maxPower#

int16_t RAIL_TxPowerCurves_t::maxPower

max deci-dBm value


Definition at line 87 of file plugin/pa-conversions/pa_curve_types_efr32.h

minPower#

int16_t RAIL_TxPowerCurves_t::minPower

min deci-dBm value


Definition at line 89 of file plugin/pa-conversions/pa_curve_types_efr32.h

powerParams#

const RAIL_TxPowerCurveSegment_t* RAIL_TxPowerCurves_t::powerParams

Pointer to "piecewiseSegments"-length array of RAIL_TxPowerCurveSegment_t of power (deci-dBm) to powerLevel conversion fits.


Definition at line 95 of file plugin/pa-conversions/pa_curve_types_efr32.h