RAIL sync words and length configuration.
DeprecatedRAIL 2.x synonym of sl_rail_sync_word_config_t.
Public Attributes#
uint8_t
Sync word length in bits, between 2 and 32, inclusive.
uint32_t
Sync Word1.
uint32_t
Sync Word2.
Public Attribute Documentation#
syncWordBits#
uint8_t RAIL_SyncWordConfig_t::syncWordBits
Sync word length in bits, between 2 and 32, inclusive.
DeprecatedRAIL 2.x synonym of sl_rail_sync_word_config_t::sync_word_bits.
syncWord1#
uint32_t RAIL_SyncWordConfig_t::syncWord1
Sync Word1.
Note
Only the least-significant syncWordBits bits are used, which are sent or received on air least-significant-bit first.
DeprecatedRAIL 2.x synonym of sl_rail_sync_word_config_t::sync_word_0.
syncWord2#
uint32_t RAIL_SyncWordConfig_t::syncWord2
Sync Word2.
Note
Only the least-significant syncWordBits bits are used, which are sent or received on air least-significant-bit first.
DeprecatedRAIL 2.x synonym of sl_rail_sync_word_config_t::sync_word_1.