A configuration structure for a scheduled transmit.

Public Attributes#

The time when to transmit this packet.

The type of delay.

Indicate which action to take with a scheduled TX if it occurs during RX.

Public Attribute Documentation#

when#

sl_rail_time_t sl_rail_scheduled_tx_config_t::when

The time when to transmit this packet.

The exact interpretation of this value depends on the mode specified below.


mode#

sl_rail_time_mode_t sl_rail_scheduled_tx_config_t::mode

The type of delay.

See the sl_rail_time_mode_t documentation for more information. Be sure to use SL_RAIL_TIME_ABSOLUTE delays for time-critical protocols.


tx_during_rx#

sl_rail_scheduled_tx_during_rx_t sl_rail_scheduled_tx_config_t::tx_during_rx

Indicate which action to take with a scheduled TX if it occurs during RX.

See sl_rail_scheduled_tx_during_rx_t structure for more information on potential options.