WiSeConnect - Network Stack Version 4.1.2 (Oct 14, 2026) - Release Notes#
Wi-Fi 6 + BLE (WiSeConnect) SDK Version 4.1.2
Simplicity SDK Version 2026.6.2
The Network Stack Software Development Kit (SDK) provides core and advanced networking features with Wi-Fi IoT cloud integration.
See WiSeConnect releases for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 4.1.2#
Added Server Name Indication (SNI) support for HTTPS PUT requests.
Added in 4.1.1#
None
Added in 4.1.0#
New TCP/TLS advanced-configuration setters for the HTTP client, MQTT client, and WebSocket client services.
Dual-stack (IPv4 + IPv6) network manager consolidation in
sl_net_for_dual_stack.c.
API Changes#
Added in 4.1.2#
None
Added in 4.1.1#
New
sl_websocket_set_origin()added to inject a custom HTTPOriginheader during WebSocket connection establishment, enabling clients to comply with cross-origin resource sharing (CORS) requirements or to test server-side origin checks.New
sl_wifi_get_ip_config_failure_reason(sl_status_t *ipv4_status, sl_status_t *ipv6_status)API added to retrieve per-family IPv4/IPv6 IP configuration status from the last bring-up attempt, including partial-success and dual-stack failure diagnostics.
Added in 4.1.0#
New
sl_http_client_set_tcp_tls_advanced_configuration(),sl_mqtt_client_set_tcp_tls_advanced_configuration(), andsl_websocket_set_tcp_tls_advanced_configuration()setters.NETWORK_ERROR_TLS_HOSTNAME_REQUIREDadded for embedded MQTT TLS flows (MQTTSi91x_lwip.h); HTTP/MQTT/WebSocket TCP-TLS advanced configuration returnsSL_STATUS_INVALID_PARAMETERwhen TLS-SNI is enabled without a hostname.sl_net_dns_resolve_hostname()flagged withSL_DEPRECATED_API_WISECONNECT_4_1.
Bug Fixes#
Fixed in 4.1.2#
Fixed a data stall in CoEx TCP_RX mode with the 352_320K memory retention configuration where the DUT stopped printing throughput logs after the async receive test started.
Fixed an issue that could cause HTTPS GET operations to become unresponsive or return truncated data when the remote server closed the connection before the full response reached the host.
Fixed an infinite MQTT disconnect event loop that occurred when the network or broker became unavailable after a successful MQTT connection.
Fixed SNTP month-string parsing so that August is correctly reported as
"Aug"instead of"Aud".Fixed an issue where
NULLwas returned to the HTTP client during final HTTPS PUT server-response callbacks in the event handler.Fixed remote-termination handling to report the host BSD socket descriptor and remote peer port, instead of the firmware socket ID and local port.
Fixed host–NWP timestamp synchronization, feature frame handling, and AWS MQTT reliability during power-save operation.
Fixed SI91x
select()disconnect handling to recognize peer-disconnect events and log"Client closed connection"instead of reporting a false select failure.Fixed a race where remote termination (
0x62) could prematurely complete in-flight socket close or read operations, leaving socket state inconsistent when the firmware response arrived later.
Fixed in 4.1.1#
Fixed an issue where MQTT messages containing null or empty payloads were not being received or processed correctly.
Fixed an issue where the DUT did not respond on a TCP server socket when the remote peer closed the connection with FIN during data transfer.
Fixed a TCP_RX socket connection failure after BLE was disabled in the CoEx throughput application when the remote peer did not complete the FIN/ACK handshake in a prior connection close.
Fixed
sl_net_get_ip_address()to return the configured static IP address in static mode and the DHCP-assigned IP address in DHCP mode.Fixed
sl_si91x_bind(port=0)to correctly allocate ephemeral local ports for zero-valued bind requests.Fixed dual-IP profile connectivity on IPv4-only networks by allowing APIs to return IPv4/IPv6 partial-success codes when IPv6 connection fails.
Fixed the Wi-Fi Throughput example to correctly enforce configured timeout handling in the async RX wait loop when iperf is terminated mid-test during async UDP/TCP RX testing.
Fixed in 4.1.0#
Fixed stability issues in select() timeout handling when both read and write file descriptor sets are specified together.
Fixed stability issues in select() when the timeout is set to 0 while operating on an SSL-enabled socket.
LWIP MQTT (
paho_mqtt_client/lwip_mqtt_over_tcp) MQTTS flow now requiresNetworkSetTlsHostname()beforeNetworkConnect(), handlesNETWORK_ERROR_TLS_HOSTNAME_REQUIRED, and performs full TLS/TCP cleanup on errors.Dual-stack (IPv4 + IPv6) NWP/M4 example: UDP IPv6 transfer fix and dual-stack errors under
LWIP_IPV4=0/LWIP_SOCKET=0.
Chip Enablement#
Added in 4.1.2#
None
Added in 4.1.1#
None
Added in 4.1.0#
None
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces applicable for each feature.
New Features#
Added in 4.1.2#
Added Server Name Indication (SNI) support for HTTPS PUT requests.
Added in 4.1.1#
None
Added in 4.1.0#
BLE memory can now be reused for Network Stack memory and packet buffers once BLE is disabled.
Fixed race conditions in the socket closure path when remote termination and local socket close occur simultaneously.
Added support for graceful TCP FIN handshake closure.
Improved stability in the rejoin and IP-change handling paths.
Improved stability in concurrent (STA + AP) mode.
Upgraded the lwIP stack from v2.1.2 to v2.2.1.
Configurable TCP Parameters – Added configuration options for TCP retransmission count and TCP keep-alive count.
HTTP / MQTT / WebSocket TCP-TLS advanced configuration: New public setters on the three service clients allow configuration of TCP and TLS advanced options (for example, TLS-SNI hostname).
Dual-stack consolidation:
components/service/network_manager/src/sl_net_for_dual_stack.cconsolidates the IPv4 + IPv6 paths used by network-manager examples.
Enhancements#
Added in 4.1.2#
None
Added in 4.1.1#
Enhanced WebSocket configuration by making the Origin header configurable instead of hardcoded to http://localhost, improving deployment flexibility and interoperability.
Added support for MQTT client port 0 and use configured port.
Added configurable ALPN support in MQTT-over-TLS (including port 443 use cases), with strict TLS extension TLV validation and consistent errno mapping across BSD/LwIP paths.
Added in 4.1.0#
Embedded MQTT TLS flows require
NetworkSetTlsHostname()before connect; missing hostname returnsNETWORK_ERROR_TLS_HOSTNAME_REQUIRED.HTTP/MQTT/WebSocket TCP-TLS advanced configuration validates TLS-SNI hostname and returns
SL_STATUS_INVALID_PARAMETERwhen required but unset.Added specific TLS/SSL handshake failure error codes to distinguish certificate, trust, hostname, and protocol mismatch failures beyond the generic handshake-failed (0xBBD2) error when debugger logging is enabled.
Removed Features#
Removed in 4.1.2#
None
Removed in 4.1.1#
None
Removed in 4.1.0#
None
Deprecated Features#
Deprecated in 4.1.2#
None
Deprecated in 4.1.1#
None
Deprecated in 4.1.0#
None
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added in 4.1.2#
None
Added in 4.1.1#
New API Signature | Deprecated API replaced by this (if any) |
|---|---|
| None |
| None |
Added in 4.1.0#
New API Signature | Deprecated API replaced by this (if any) |
|---|---|
| None |
| None |
| None |
|
|
Modified APIs#
Modified in 4.1.2#
None
Modified in 4.1.1#
None
Modified in 4.1.0#
Modified API / Type | Change Description |
|---|---|
| New advanced-config option structures added in the matching |
Removed APIs#
Removed in 4.1.2#
None
Removed in 4.1.1#
None
Removed in 4.1.0#
None
Deprecated APIs#
Deprecated in 4.1.2#
None
Deprecated in 4.1.1#
None
Deprecated in 4.1.0#
The following Net-Stack public APIs are newly marked with SL_DEPRECATED_API_WISECONNECT_4_1 (legacy kept as an alias; define SL_SUPPRESS_DEPRECATION_WARNINGS_WISECONNECT_4_1 to suppress warnings while migrating).
Deprecated API Name | Planned Removal Date |
|---|---|
| 2028-12 |
Bug Fixes#
Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.
Fixed in 4.1.2#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, OPNs, Boards, Modes, Host Interfaces |
|---|---|---|---|
| 1757221 | Fixed an issue that could cause HTTPS GET operations to become unresponsive or return truncated data when the remote server closed the connection before the full response reached the host. | None |
|
| 1778912 | Fixed an infinite MQTT disconnect event loop that occurred when the network or broker became unavailable after a successful MQTT connection. | None |
|
| 1783374 | Fixed SNTP month-string parsing so that August is correctly reported as "Aug" instead of "Aud". |
None |
|
| 1752441 | Fixed an issue where NULL was returned to the HTTP client during the final HTTPS PUT server-response callbacks in the event handler. |
None |
|
| 1751379 | Fixed remote-termination handling to report the host BSD socket descriptor and remote peer port instead of the firmware socket ID and local port. | None |
|
| 1704878, 1757236 | Fixed host–NWP timestamp synchronization, feature frame handling, and AWS MQTT reliability during power-save operation. | None |
|
| 1739922 | Fixed SI91x select() disconnect handling to detect peer disconnection events and log "Client closed connection" instead of incorrectly reporting a select failure. |
None |
|
| 1686801 | Fixed a race condition where remote termination (0x62) could prematurely complete in-flight socket close or read operations, leaving socket state inconsistent when the firmware response arrived. |
None |
|
Fixed in 4.1.1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, OPNs, Boards, Modes, Host Interfaces |
|---|---|---|---|
| 1683916 | Fixed an issue where MQTT messages containing null or empty payloads were not being received or processed correctly. | None |
|
| 1681789 | Fixed an issue where the DUT did not respond on a TCP server socket when the remote peer closed the connection with FIN during data transfer. | None |
|
| 1672602 | Fixed a TCP_RX socket connection failure after BLE was disabled in the CoEx throughput application when the remote peer did not complete the FIN/ACK handshake in a prior connection close. | None |
|
| 1625569 | Fixed sl_net_get_ip_address() to return the configured static IP address in static mode and the DHCP-assigned IP address in DHCP mode. |
None |
|
| 1678276 | Fixed sl_si91x_bind(port=0) to correctly enable ephemeral local-port allocation by bypassing fixed-port collision validation for zero-valued bind requests. |
None |
|
| 1681637 | Fixed dual-IP profile connectivity on IPv4-only networks by allowing APIs to return IPv4/IPv6 partial-success codes when IPv6 connection fails. | None |
|
| 1660782 | Fixed the Wi-Fi Throughput example to correctly enforce configured timeout handling in the async RX wait loop when iperf is terminated mid-test during async UDP/TCP RX testing. | None |
|
Fixed in 4.1.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, OPNs, Boards, Modes, Host Interfaces |
|---|---|---|---|
| N/A | LWIP MQTT (paho_mqtt_client/lwip_mqtt_over_tcp) MQTTS flow now requires NetworkSetTlsHostname() before NetworkConnect(), handles NETWORK_ERROR_TLS_HOSTNAME_REQUIRED, and performs full TLS/TCP cleanup on errors. |
None |
|
| N/A | Compilation fix on the LWIP MQTT path. | None |
|
| N/A | Dual-stack errors under LWIP_IPV4=0 / LWIP_SOCKET=0 fixed in the dual-stack example. |
None |
|
| N/A | UDP IPv6 transfer fix in the dual-stack NWP/M4 example. | None |
|
| 1533360 | Fixed the BSD error 48 (socket bind failure) in the paho_mqtt_client/mqtt_over_tcp example during extended operation with repeated connect and disconnect cycles. | None |
|
| 1586929 | Resolved SLCP compilation errors in the wifi_net_dual_stack_nwp_m4 example when both netX and LwIP components are included. |
None |
|
| 1438843 | Fixed an issue where HTTP server became unresponsive after an iPhone browser closed the connection before completing a request. | None |
|
| 1466146 | Fixed multithread-sockets TCP_RX teardown order so the client socket is closed before the server socket, preventing the spurious client-close failure. | None |
|
| 1502295 | Fixed an issue where select_given was incorrectly set when sl_si91x_select() was not registered for a select slot, preventing the application from assuming a select is active when firmware rejected the request. |
None |
|
| 1612990 | Updated the embedded MQTT examples to handle MQTT receive error cases (SL_MQTT_CLIENT_MAX_RX_PAYLOAD_SIZE exceeded, allocation failure, or corrupted reassembly) in the error in the event handler. |
None |
|
| 1615135 | Fixed an issue in RAW_DATA socket-to-host mapping that could cause missed WebSocket ping responses and unstable connection closure behavior. | None |
|
| 1614539 | Fixed an issue where the lwIP TCP client snippet could not handle TX backpressure: paces sends, retries transient send() errors (ENOBUFS / EAGAIN / EWOULDBLOCK), and connection instability. |
None |
|
| 1630112 | Fixed an issue where sli_net_get_vap_for_ip_version() could return EAFNOSUPPORT when no sl_net profile was available and the application configured IP addresses directly by using sl_si91x_configure_ip_address(). | None |
|
| 1639986 | Fixed an issue where HTTP PUT operation could fail on completion because of TCP connection teardown handling. | None |
|
| 1402920 | Fixed the TCP server bind failure on re-run in the Wi-Fi Select app, so that fd 0 (a legal descriptor) is no longer skipped. |
None |
|
| 1587427 | Removed dead code in HTTP ABORT/HTTP CLIENT PUT response handling that could never run and would have double-freed a buffer. No behavior change; fix is cleanup and safety. | None |
|
| 1647932 | Fixed memory leaks in ECDSA crypto processing for the firmware crypto command. | None |
|
| 1629554 | Fixed the stability issues in select() timeout handling when both read and write file descriptor sets were specified together. | None |
|
| 1625105 | Fixed the stability issues in select() when a timeout value of 0 was used with an SSL-enabled socket. | None |
|
| 1641898 | Fixed an issue where DHCP IP address assignment validation could fail after redirecting IPv4 and IPv6 address output from printf to SL_DEBUG_LOG_V2. | None |
|
Chip Enablement#
Added in 4.1.2#
None
Added in 4.1.1#
None
Added in 4.1.0#
None
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.
New Examples#
Added in 4.1.2#
None
Added in 4.1.1#
None
Added in 4.1.0#
None
Modified Examples#
Modified in 4.1.2#
| Example Name | Changes | Supported Software Variants (if applicable) | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Wi-Fi - HTTPS PUT Example See README |
Updated to support Server Name Indication (SNI) for HTTPS PUT requests. The example now demonstrates SNI hostname configuration and PUT operations to SNI-enabled servers. | Standard and Lite |
|
|
SPI, UART |
|
Wi-Fi - MQTT(TLS) Example See README |
MQTT client profiles configured with both IPv4 and IPv6 now return partial-success and dual-stack error codes when either IP family fails. Improved diagnostics for connection failures and hostname/SNI configuration validation. | Standard and Lite |
|
|
SPI, UART |
|
Wi-Fi - HTTP Client Example See README |
Improved handling and reporting of remote-termination and BSD socket errors; context user pointers now preserved for HTTPS PUT callbacks. Enhanced TLS SNI and host validation. | Standard and Lite |
|
|
SPI, UART |
|
Wi-Fi - TCP Throughput Example See README |
Resolved an issue in CoEx TCP_RX mode for the 352_320K memory retention configuration that previously caused the device to become unresponsive during async RX tests after BLE was disabled; throughput logging now operates as expected. Improved error handling and resource cleanup in TCP close scenarios. | Standard and Lite |
|
|
SPI, UART |
|
Wi-Fi - WebSocket Client Example See README |
Now supports setting Origin header programmatically (not hardcoded) and additional diagnostics for connection and TLS errors; maintains support for SNI and enhanced dual-stack (IPv4/IPv6) reporting. | Standard and Lite |
|
|
SPI, UART |
Modified in 4.1.1#
| Example Name | Changes | Supported Software Variants (if applicable) | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Wi-Fi - WebSocket Client See README |
Aligned with the new WebSocket origin-capable client path, allowing the Origin header to be set programmatically instead of using a hardcoded value. | Standard and Lite |
|
|
SPI, UART |
Modified in 4.1.0#
| Example Name | Changes | Supported Software Variants (if applicable) | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Wi-Fi - Embedded MQTT Client, Embedded MQTT Client TWT See README |
Now handle MQTT-RX errors (receive-failed, payload exceeding SL_MQTT_CLIENT_MAX_RX_PAYLOAD_SIZE, allocation failure, corrupted reassembly) via a new mqtt_client_error_event_handler instead of always terminating. |
Standard and Lite |
|
|
SPI, UART |
|
Wi-Fi - Paho LWIP MQTT over TCP See README |
Updated for the MQTTS hostname-required flow and full TLS/TCP cleanup on errors. | Standard and Lite |
|
|
SPI, UART |
|
Wi-Fi - SNTP, HTTP OTAF, HTTP OTAF TWT, M4 Firmware Update, Bootloader XModem See README |
Migrated to sl_net_dns_resolve_hostname_v2 (timeout / retry). |
Standard and Lite |
|
|
SPI, UART |
|
Wi-Fi - Cloud Apps, Provisioning, Three SSL Concurrent Client Sockets See README |
Aligned with the new HTTP/MQTT/WebSocket TCP-TLS advanced-configuration APIs. | Standard and Lite |
|
|
SPI, UART |
Removed Examples#
Removed in 4.1.2#
None
Removed in 4.1.1#
None
Removed in 4.1.0#
None
Deprecated Examples#
Deprecated in 4.1.2#
None
Deprecated in 4.1.1#
None
Deprecated in 4.1.0#
None
Known Issues and Limitations#
Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.
Added in 4.1.2#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, OPNs, Boards, Modes, Host Interfaces |
|---|---|---|---|---|
| 1818465 | The MQTT client may not deliver SL_MQTT_CLIENT_DISCONNECTED_EVENT when the network is abnormally disconnected. |
None | None |
|
| 1827728 | In the default Paho MQTT client examples (mqtt_over_tcp, lwip_mqtt_over_tcp, and mqtt_over_websocket), MQTT messages are received successfully, but the Receive Data Success log is printed at DEBUG level and is not visible at the default INFO log level, which can make it appear that message receive failed. |
None | Change the Receive Data Success log from DEBUG to INFO in the Paho MQTT example applications, or enable DEBUG logging. Message receive can also be confirmed from the Message: printf output. |
|
Added in 4.1.1#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, OPNs, Boards, Modes, Host Interfaces |
|---|---|---|---|---|
| 1692587 | Throughput numbers may vary when measured with iperf running on Windows compared with Linux. Lower throughput is typically observed on Windows, particularly for TCP TX/RX and AP-mode UDP RX. | None | None |
|
Added in 4.1.0#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, OPNs, Boards, Modes, Host Interfaces |
|---|---|---|---|---|
| 1607288 | When IPv6 is enabled with LwIP timer optimization, the DUT may take more than 30 seconds to join certain access points. This behavior is observed only with specific AP models. | None | None |
|
| 745282 | Occasionally, during a TLS handshake, the device generates incorrect ECC curve parameters, causing a connection failure that results in a BBD2 error. |
None | The error is recovered in the next attempt. |
|
| 1651053 | HTTPS download may fail with error code 0x7 on certain APs in IOP scenarios. | None | None |
|
| 1675400 | Dual simultaneous AWS MQTT/TLS sessions may fail to establish after BLE is disabled with reclaimed BLE memory. | None | None |
|
| 1681637 | When the Wi-Fi client profile is configured with both IPv4 and IPv6 enabled (SL_IPV4 | SL_IPV6, typically with SL_IP_MANAGEMENT_DHCP), connection to an access point that does not provide IPv6 service fails completely. The device returns SL_STATUS_SI91X_DHCPV6_HANDSHAKE_FAIL (0x1BB9C) and does not remain operational on IPv4, even though IPv4 DHCP could have succeeded. |
None | Configure the Wi-Fi client profile for IPv4 only (SL_IPV4) when connecting to IPv4-only access points. |
|
| 1625569 | When the device is configured with static IP using SL_IP_MANAGEMENT_STATIC_IP, it still operates as a DHCP client after connecting to the network. sl_net_get_ip_address() returns a DHCP-assigned IP address instead of the configured static IP. |
None | Use the static IP directly from the Wi-Fi client profile configuration instead of relying on sl_net_get_ip_address(). |
|
| 1661749 | MQTT over TLS on port 443 with Application-Layer Protocol Negotiation (ALPN) may fail with error 12 (cannot allocate memory) when ALPN configuration is added to the Paho MQTT over TCP application. | None | None |
|
| NA | The power-saving benefits of the hosted Network Stack LWIP may not be fully realized when IPv6 mode is enabled if the network infrastructure lacks IPv6 support. | None | None |
|
| NA | External connections to services hosted within the NAT environment are not supported. | None | None |
|
| NA | NAT/PAT is incompatible with protocols and applications that embed IP address and port number information within the payload (examples include SMTP, SNMP, and similar protocols). | None | None |
|
| NA | Network traffic translation and additional processing requirements result in increased latency and reduced throughput performance. | None | None |
|
| NA | Inbound traffic routing is not supported by the current implementation. | None | None |
|
| NA | Outbound ICMP traffic (ping requests) is restricted to a maximum payload size of 300 bytes. | None | None |
|
| N/A | TLS or DTLS connections must be initiated sequentially after the completion (success or failure) of the previous connection. | None | None |
|
| N/A | Power save with TCP/IP is not supported with the UART host interface in the non-bypass mode. | None | None |
|
| N/A | Embedded MQTT usernames are supported only up to 120 bytes. | None | None |
|
| N/A | Embedded MQTT topic lengths are supported only up to 200 bytes. | None | None |
|
| N/A | Embedded MQTT passwords are supported only up to 62 bytes. | None | None |
|
| N/A | HTTP GET URL lengths are only supported up to 2048 bytes. | None | None |
|
| N/A | More than three SSL connections are not supported. | None | None |
|
| N/A | The combined length of the mDNS service type and instance name is limited to 30 bytes maximum. | None | None |
|
| 1660782 | In the Wi-Fi Throughput example, if the iperf session is stopped abruptly (for example, force-closed from the PC), the application may not recover as expected. TCP RX and UDP RX tasks can get stuck and not exit even after the configured timeout. TCP RX may return immediately. | None | Avoid force-killing iperf during a throughput test—stop the test normally or let it finish. If the app hangs, reset the device before running the next test. |
|
| 1678276 | Calling sl_si91x_bind() with port 0 (to let the system pick a free port) fails with error 40 (address already in use). This affects UDP client setups that need a dynamically assigned local port, such as bidirectional UDP with one fixed server port and one client socket. A fix is planned in an upcoming release. |
None | Use a fixed local port in bind(), or call send() after socket creation so the port is assigned automatically without binding to port 0. |
|
| 1680037 | The sl_mqtt_version_t enum lists only MQTT v3.0 and v3.1, even though the MQTT client supports v3.1.1. Because of this, it is unclear which value to set in the client configuration passed to sl_mqtt_client_connect_v1(). A documentation and API update is planned in an upcoming release. |
None | Use SL_MQTT_VERSION_3_1 for MQTT v3.1.1 connections until the enum is updated. |
|
| 1660224 | In concurrent STA+AP mode, an active MQTT session on the STA interface is dropped when the AP interface is brought down (e.g., via wifi_down). This occurs when MQTT traffic runs on STA while the device is operating in concurrent mode and the AP interface is stopped. A fix is planned in an upcoming release. |
None | Avoid toggling the AP interface while MQTT is active on STA, or restart the MQTT session after AP changes. |
|
| 1678345 | When Wi-Fi TCP traffic runs together with Secure GPIO control and periodic set power-state changes, the device may return SL_STATUS_SI91X_COMMAND_GIVEN_IN_INVALID_STATE after several hours of continuous operation. This was seen on secure-zone enabled setups where GPIO pins toggle while TCP transmit runs in a loop with power save enabled. |
None | Limit concurrent Wi-Fi, GPIO, and power-save activity in secure applications, or reset the device if this error occurs. |
|