Edit

WiSeConnect - SiWx91x Platform SDK Version 4.1.2 (Oct 14, 2026) - Release Notes#

Wi-Fi 6 + BLE (WiSeConnect) SDK Version 4.1.2

Simplicity SDK Version 2026.6.2

The SiWx91x Platform Software Development Kit (SDK) provides platform features for Silicon Labs SiWx91x microcontrollers, including peripherals, drivers, and services.

See WiSeConnect releases for earlier releases.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 4.1.2#

  • Added SDK support for 16 MB flash.

  • Added SDK support for the EOL Sensors board BRD2605B.

  • Added LTO support for PSRAM-enabled applications compiled using the LLVM or GCC toolchain.

Added in 4.1.1#

None

Added in 4.1.0#

  • Added a Memory Manager Redirect component to redirect libc heap allocations to the CMSIS FreeRTOS heap_4 allocator by using heap wrappers.

  • Added support for a programmable I2C SDA hold time.

API Changes#

Added in 4.1.2#

None

Added in 4.1.1#

None

Added in 4.1.0#

  • sl_status_t sl_si91x_secure_storage_write_register(mcu_secure_storage_register_t register_index, uint32_t value);

  • sl_status_t sl_si91x_secure_storage_read_register(mcu_secure_storage_register_t register_index, uint32_t *value);

  • sl_status_t sl_si91x_secure_storage_enable_protection_and_lock(void);

Bug Fixes#

Fixed in 4.1.2#

  • Fixed an issue where Sideband GCM and CMAC could fail when no additional data was provided.

  • Fixed an issue where SiWx917 UART1 TX pin selection allowed unsupported GPIO_34 values, causing compilation failures.

  • Fixed an issue where ECDSA signature verification could fail when using GCC with LTO.

  • Fixed an issue where sl_si91x_nwp_soft_reset_from_updater() could leave the M4 Security Updater application unresponsive and and prevent the function from returning.

  • Fixed SLC validation failures in WiseConnect with Simplicity SDK 2026.6.0.

  • Fixed an issue where sl_wifi_deinit() could fail or leave the device unresponsive after several Wi-Fi + BLE coexistence initialization and deinitialization cycles.

  • Fixed a discrepancy in the SDIO application block-size configuration of 512.

  • Fixed an issue where Sideband crypto buffer alignment did not comply with the PSA Crypto API specification.

  • Fixed an issue where the AES-GCM decryption output buffer could overrun by 16 bytes.

Fixed in 4.1.1#

  • Fixed SLC validation failures when using WiseConnect with Simplicity SDK 2026.6.0.

  • Fixed an issue where the sl_si91x_mic application did not work when GCC LTO was enabled on the BRD2605A dev kit.

  • Fixed an implementation issue in the sl_si91x_adc_read_data_static() function.

  • Fixed an issue where the UART RS485 bare-metal and FreeRTOS applications did not work as expected on the BRD4342A PSRAM board.

  • Fixed an issue where sideband crypto did not work when input data was stored in flash memory.

  • Fixed an issue where debug prints did not work in projects created from an OPN when the Debug UC component was installed and ULP UART was enabled.

  • Fixed an issue where ChaCha20-Poly1305 operations with sideband crypto failed for payloads larger than 144 bytes.

  • Fixed intermittent NWP issues observed during AE + TCP maximum stress testing when logging was enabled.

  • Updated the SiWx91x Platform QEI example README to clarify hardware requirements and pin configuration guidance.

  • Updated the Hardware Requirements section by adding BRD4343C details and removing duplicate OPN entries.

  • Fixed an issue where SSI FreeRTOS primary and secondary data mismatched on the primary side on BRD4342A.

  • Fixed memory leak in the sli_memlcd_spi_tx() API.

  • Fixed an issue that could occur when switching between STA and AP modes due to unintended log activity during shutdown and unsynchronized updates to P2P status registers.

Fixed in 4.1.0#

  • Updated platform driver files to remove direct inclusion of FreeRTOS header files.

  • Removed the obsolete GY61 multichannel ADC sensor entry from sensorhub_config.c.

  • Fixed Si7021 sensor initialization failures with sleepy Matter applications.

  • Deprecated power manager APIs.

  • Fixed GPIO wrapper behavior to prevent output from being forced low and to allow configuration of the initial GPIO state.

  • Updated the information about ADC sample rate range in WiSeConnect SDK ADC examples and release notes.

  • Fixed I2C application behavior after waking up from calendar-based sleep.

  • Fixed HSPI secondary DMA loopback data corruption with 256-byte block size.

  • Enhanced peripheral component and README documentation.

  • Resolved documentation conflict for ULP_UART hardware flow control support.

Chip Enablement#

Added in 4.1.2#

  • Added support for the BRD2605B radio board.

Added in 4.1.1#

None

Added in 4.1.0#

  • New radio boards added: BRD4343C

  • New chip components added: siwg917y110lgaxa, siwg917y110lgnxa, siwg917y111mgaxa, siwg917y111mgnxa, siwg917y121mgnxa, siwg917y121mgaxa

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces applicable for each feature.

New Features#

Added in 4.1.2#

  • Added SDK support for 16 MB flash.

  • Added SDK support for the EOL Sensors board BRD2605B.

  • Added LTO support for PSRAM-enabled applications compiled using the LLVM or GCC toolchain.

Added in 4.1.1#

None

Added in 4.1.0#

  • Added DCH message type for ml_profiler on Si917.

  • Upgraded GCC to 14.2 and enabled Link Time Optimization (LTO) for GCC-based builds.

  • Added SDK support for SiWG917Y module refresh variants and XMC 8MB Flash boards.

  • Updated SiWx91x platform code to support BRD4002B Mainboard with EFR Driver Integration.

  • Incorporated the ARM CMSIS upgrade from v5.8 to v6.2 as part of the Simplicity SDK update used by WiSeConnect sample apps.

  • Added a Memory Manager Redirect component to redirect libc heap allocations to the CMSIS FreeRTOS heap_4 allocator by using heap wrappers.

  • Enabled sideband support for PSA crypto. (Note: Supported with PSA APIs and input buffers with M4 RAM).

  • Debug logger:

    • SystemView is integrated.

    • Debug Logger logging is not enabled by default for the NWP. Users who require Debug Logger logs must enable them manually by following the instructions provided in the SRM.

    • Enabled IO Stream backend support (VCOM, RTT) on the SiWx917 platform.

Enhancements#

Added in 4.1.2#

None

Added in 4.1.1#

None

Added in 4.1.0#

  • Improved PSRAM application support with updated jinja and linker configurations, a dedicated .log_fmt section, and IO stream trace support for ML profiling.

  • Updated peripheral application and component names from si91x to SiWx91x for naming consistency.

  • Decoupled PSRAM Core and PSRAM Device components, enabling independent component selection.

  • Updated the SiWx917 SVD file to incorporate the latest HRM changes and ensure alignment with the current register definitions.

  • Updated Startup and PSRAM linker files.

Removed Features#

Removed in 4.1.2#

None

Removed in 4.1.1#

None

Removed in 4.1.0#

None

Deprecated Features#

Deprecated in 4.1.2#

None

Deprecated in 4.1.1#

None

Deprecated in 4.1.0#

None

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 4.1.2#

None

Added in 4.1.1#

None

Added in 4.1.0#

New API Signature

Deprecated API replaced by this (if any)

sl_i2c_driver_configure_sda_hold_time

None

sl_si91x_secure_storage_write_register

None

sl_si91x_secure_storage_read_register

None

sl_si91x_secure_storage_enable_protection_and_lock

None

sl_si91x_pcm_config_transmit_receive

None

sl_si91x_pcm_transfer

None

sl_si91x_i2s_transfer

None

sl_gpio_pin_configure_gpio_output_level

None

sl_si91x_iostream_set_console_instance

None

sl_status_t sl_si91x_adc_configure_clock

None

SLI_SI91X_POWER_MANAGER_CORE_ENTER_CRITICAL()

sl_si91x_power_manager_core_entercritical

SLI_SI91X_POWER_MANAGER_CORE_EXIT_CRITICAL(irq_state)

sl_si91x_power_manager_core_exitcritical

SL_DEBUG_LOG_V2(...)

dummy_printf

Modified APIs#

Modified in 4.1.2#

None

Modified in 4.1.1#

None

Modified in 4.1.0#

None

Removed APIs#

Removed in 4.1.2#

None

Removed in 4.1.1#

None

Removed in 4.1.0#

None

Deprecated APIs#

Deprecated in 4.1.2#

None

Deprecated in 4.1.1#

None

Deprecated in 4.1.0#

Deprecated API Name

Replacement

Planned Removal Date

sl_si91x_power_manager_sleep

sli_si91x_power_manager_sleep

2028-06

sl_si91x_power_manager_standby

sli_si91x_power_manager_standby

2028-06

sl_si91x_power_manager_core_entercritical

SLI_SI91X_POWER_MANAGER_CORE_ENTER_CRITICAL

2028-06

sl_si91x_power_manager_core_exitcritical

SLI_SI91X_POWER_MANAGER_CORE_EXIT_CRITICAL

2028-06

void dummy_printf(const char *fmt, ...)

SL_DEBUG_LOG_V2(...)

2028-06

sl_si91x_adc_configure_clock

—

2028-06

Bug Fixes#

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

Fixed in 4.1.2#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
1791107 Fixed an issue where Sideband GCM and CMAC could fail when no additional data was provided. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1787489 Fixed an issue where SiWx917 UART1 TX pin selection allowed unsupported GPIO_34 values, causing compilation failures. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1751704 Fixed an issue where ECDSA signature verification could fail when using GCC with LTO. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1750268 Fixed an issue where sl_si91x_nwp_soft_reset_from_updater() could leave the M4 Security Updater application unresponsive and prevent the function from returning. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1703676 Fixed SLC validation failures in WiseConnect with Simplicity SDK 2026.6.0. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1660521 Fixed an issue where sl_wifi_deinit() could fail or leave the device unresponsive after several Wi-Fi and BLE coexistence initialization and deinitialization cycles. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1827902 Fixed a discrepancy in the SDIO application block-size configuration of 512. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1694702 Fixed an issue where Sideband crypto buffer alignment did not comply with the PSA Crypto API specification. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1734857 Fixed an issue where the AES-GCM decryption output buffer can overrun by 16 bytes. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A

Fixed in 4.1.1#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
1685461 Fixed SLC validation failures when using WiseConnect with Simplicity SDK 2026.6.0. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1682446 Fixed an issue where the sl_si91x_mic application did not work when GCC LTO was enabled on the BRD2605A dev kit. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: BRD2605A
  • Modes: SoC
  • Host interfaces: N/A
1533235 Fixed an implementation issue in the sl_si91x_adc_read_data_static() function. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1676598 Fixed an issue where the UART RS485 bare-metal and FreeRTOS applications did not work as expected on the BRD4342A PSRAM board. None
  • Software variants: Standard and Lite
  • OPNs: All SiWG917 PSRAM-supported OPNs
  • Boards: BRD4342A
  • Modes: SoC
  • Host interfaces: N/A
1693912 Fixed an issue where sideband crypto did not work when input data was stored in flash memory. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1716168 Fixed an issue where debug prints did not work in projects created from an OPN when the Debug UC component was installed and ULP UART was enabled. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1731250 Fixed an issue where ChaCha20-Poly1305 operations with sideband crypto failed for payloads larger than 144 bytes. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1638463 Fixed intermittent NWP issues observed during AE + TCP maximum stress testing when logging was enabled. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1681802 Updated the SiWx91x Platform QEI example README to clarify hardware requirements and pin configuration guidance. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1680783 Updated the Hardware Requirements section by adding `BRD4343C` details and removing duplicate OPN entries. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: BRD4343C
  • Modes: SoC
  • Host interfaces: N/A
1670638 Fixed SSI FreeRTOS primary/secondary data mismatch observed on the primary side on BRD4342A. None
  • Software variants: Standard and Lite
  • OPNs: All SiWx917 PSRAM supported OPNs
  • Boards: BRD4342A
  • Modes: SoC
  • Host interfaces: N/A
1666482 Fixed memory leak in sli_memlcd_spi_tx() API. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1535468 Fixed an issue that could occur when switching between STA and AP modes due to unintended log activity during shutdown and unsynchronized updates to P2P status registers. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A

Fixed in 4.1.0#

ID Issue Description GitHub / Salesforce Reference (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
1410517 Removed direct FreeRTOS header file dependencies on the Wi-Fi SDK. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1564599 Removed the obsolete GY61 multichannel ADC sensor entry from sensorhub_config.c. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1580041 Fixed the Si7021 sensor initialization failures in the low-power (sleepy) Matter applications. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1595872 Deprecated power manager APIs. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1597421 Fixed GPIO wrapper behavior so output is not forced low and initial GPIO state can be configured. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1602498 Updated the documented ADC sample rate range in WiseConnect SDK ADC examples and release notes. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1628809 Fixed I2C application behavior after calendar-based sleep wake-up. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1634011 Fixed HSPI secondary DMA loopback data corruption with 256-byte block size. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1634996 Enhanced peripheral component and README documentation. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1646725 Removed sl_si91x_usart_set_configuration() function from the deprecated APIs list. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1638588 Added flash/FW overflow check in SoC and PSRAM linker files. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1673743 Resolved documentation conflict for ULP_UART hardware flow control support. None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A

Chip Enablement#

Added in 4.1.2#

New radio boards added:

  • BRD2605B

Added in 4.1.1#

None

Added in 4.1.0#

New radio boards added:

  • BRD4343C

New chip components are added under components/device/silabs/si91x/mcu/core/chip/component/:

  • siwg917y110lgaxa, siwg917y110lgnxa

  • siwg917y111mgaxa, siwg917y111mgnxa

  • siwg917y121mgnxa, siwg917y121mgaxa

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

New Examples#

Added in 4.1.2#

None

Added in 4.1.1#

None

Added in 4.1.0#

Example Name Description Supported Software Variants (if applicable) Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

SiWx91x Platform - ADC FIFO Mode FreeRTOS

See README

ADC FIFO example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - ADC Static Mode FreeRTOS

See README

ADC Static example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - ULP ADC FreeRTOS

See README

ULP ADC example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - Simple Button FreeRTOS

See README

Button example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - ULP Timer FreeRTOS

See README

ULP Timer example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - Empty C FreeRTOS

See README

Empty C example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - Empty Cpp FreeRTOS

See README

Empty Cpp example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - GPDMA FreeRTOS

See README

GPDMA example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - GPIO Detailed FreeRTOS

See README

GPIO Detailed example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - ULP GPIO Transition FreeRTOS

See README

ULP GPIO State Transition example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - GSPI FreeRTOS

See README

GSPI example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - Hello World FreeRTOS

See README

Hello World example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - I2C Driver Follower FreeRTOS

See README

I2C Driver Follower example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - I2C Driver Leader FreeRTOS

See README

I2C Driver Leader example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - ULP I2C Driver Leader FreeRTOS

See README

ULP I2C Driver Leader example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - I2S Loopback FreeRTOS

See README

I2S Loopback example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - I2S Primary FreeRTOS

See README

I2S Primary example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - I2S Secondary FreeRTOS

See README

I2S Secondary example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - ULP I2S FreeRTOS

See README

ULP I2S example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - Joystick FreeRTOS

See README

Joystick example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - MEMLCD FreeRTOS

See README

MEMLCD example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - PCM Loopback FreeRTOS

See README

PCM Loopback example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - PCM Primary FreeRTOS

See README

PCM Primary example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - PCM Secondary FreeRTOS

See README

PCM Secondary example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - PSRAM Blinky FreeRTOS

See README

PSRAM Blink example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All SiWx917 PSRAM supported OPNs
  • Boards: BRD4342A
N/A

SiWx91x Platform - PWM FreeRTOS

See README

PWM example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - SSI Master FreeRTOS

See README

SSI Master example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - SSI Slave FreeRTOS

See README

SSI Slave example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - ULP SSI Master FreeRTOS

See README

ULP SSI Master example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - SDIO Secondary FreeRTOS

See README

SDIO Secondary example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - SYSRTC FreeRTOS

See README

SYSRTC example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - UART FreeRTOS

See README

UART example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - UART RS485 FreeRTOS

See README

UART RS485 example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - ULP UART FreeRTOS

See README

ULP UART example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - USART Asynchronous FreeRTOS

See README

USART Asynchronous example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - USART Synchronous Master FreeRTOS

See README

USART Synchronous Master example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - USART Synchronous Slave FreeRTOS

See README

USART Synchronous Slave example application enabled with FreeRTOS on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SiWx91x Platform - I/O Stream USART FreeRTOS

See README

Iostream-over-USART service sample using sl_si91x_iostream_set_console_instance. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - MCU Secure Storage

See README

Demonstrates MCU secure storage on the SiWx91x SoC device using secure-storage register APIs sl_si91x_secure_storage_write_register, read_register, and enable_protection_and_lock. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - SHT40 Sensor

See README

Demonstrates the SHT40 temperature/humidity sensor on the SiWx91x SoC device. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - Logger Backend

See README

Demonstrates the SL_DEBUG_LOG_V2 logger backend on the SiWx91x SoC device. Standard SoC
  • OPNs: All
  • Boards: All
N/A

Modified Examples#

Modified in 4.1.2#

None

Modified in 4.1.1#

None

Modified in 4.1.0#

Example Name Changes Supported Software Variants if applicable Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

sl_si91x_pwm

See README

GPIO output level set before pin mux using sl_gpio_pin_configure_gpio_output_level. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

sl_si91x_ssi_slave

See README

SSI chip-select toggles per byte; 4343A pin documentation added. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

sl_si91x_uart, sl_si91x_usart

See UART README, USART async README

Multiple UART de-init restriction; SWO frequency correction. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

Removed Examples#

Removed in 4.1.2#

None

Removed in 4.1.1#

None

Removed in 4.1.0#

None

Deprecated Examples#

Deprecated in 4.1.2#

None

Deprecated in 4.1.1#

None

Deprecated in 4.1.0#

The following baremetal examples are deprecated in favor of their corresponding FreeRTOS examples on the SiWx91x SoC device.

Example Name Reason for Deprecation Supported Software Variants (if applicable) Supported Modes Supported OPNs / Boards / OPN Combinations Supported Host Interfaces

SL Si91x - ADC FIFO Mode

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - ADC Static Mode

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - ULP ADC

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - Button Baremetal

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - ULP Timer

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - Empty C Project SoC

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - Empty CPP Project SoC

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - GPDMA

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - GPIO Detailed Example

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - ULP GPIO State Transition Example

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - GSPI

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - Hello World

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - I2C Driver Follower

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - I2C Driver Leader

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - ULP I2C Driver Leader

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - I2S Loopback

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - I2S Primary

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - I2S Secondary

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - ULP I2S

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - IOSTREAM USART Baremetal

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - Joystick

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - MEMLCD Baremetal

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - PCM Loopback

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - PCM Primary

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - PCM Secondary

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - PSRAM Blink

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite
  • SoC
  • OPNs: All SiWx917 PSRAM supported OPNs
  • Boards: BRD4342A
N/A

SL Si91x - PWM

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - SSI Master

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - SSI Slave

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - ULP SSI Master

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - SDIO Secondary

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - SYSRTC

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - UART

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - UART RS485

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - ULP UART

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - USART Asynchronous

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - USART Synchronous Master

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

SL Si91x - USART Synchronous Slave

Deprecated in favor of the corresponding FreeRTOS example. Standard and Lite SoC
  • OPNs: All
  • Boards: All
N/A

Known Issues and Limitations#

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

Added in 4.1.2#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
1828329 When security is enabled, the device may become unresponsive if it remains in sleep mode for more than 2 seconds. None Configure the application to wake the device at least once every 2 seconds.
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1841711 Sideband Crypto does not work when the NWP is not in HIGH_PERFORMANCE mode. None Set the NWP to HIGH_PERFORMANCE mode.
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1848662 ADC threshold interrupt is not supported by the ADC driver. The driver currently supports only Static and FIFO modes. ADC threshold detection cannot be used as a PS1 wakeup source. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1830804 On the SiWG917M110LGTBA Lite OPN, M4 firmware update via TCP may fail with status 0x1 (underlying NWP status 0x1DD49, corrupted RPS header) after reading the image size. RPS flash-location validation does not correctly accept the 4 MB common-flash M4 region. None None
  • Software variants: Lite
  • OPNs: SiWG917M110LGTBA (Lite OPN)
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A

Added in 4.1.1#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
1694702 The sideband crypto buffer alignment requirement does not comply with the PSA Crypto API specification. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1734857 AES-GCM decryption can overrun the output buffer by 16 bytes. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1735621 Multipart SHA fails when multiple operations are interleaved. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A

Added in 4.1.0#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, OPNs, Boards, Modes, Host Interfaces
N/A Floating point arguments are not supported with Debug Logger. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1662836 CONFIG_MAX_ARGS values less than 3 are not supported by the Debug Logger. The minimum supported number of logger arguments is 3. None The maximum number of arguments per log call is configurable within the range of 3 to 10.
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1670763 In Coex configurations, the firmware may not report memory feasibility violations, which can result in runtime socket creation failures. The Memory Calculator correctly detects these conditions. Improvements are planned for a future release. None Use the Memory Calculator to validate memory feasibility before deployment.
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1662699 For application validation, performance measurements, and power testing, only the ERROR and WARN log levels are supported and recommended. Issues observed exclusively with the DEBUG log level should be considered debug-only observations and may not reflect normal production behavior. None Use only ERROR and WARN log levels for application validation, performance measurements, and power testing.
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
N/A NWP (Captive Core) logging is not recommended for applications using the BLE Advertising Extension (AE) feature. Do not enable SL_SI91X_ENABLE_NWP_LOGGING in the config_feature_bit_map field of sl_wifi_device_configuration_t when BLE AE is enabled. None Do not enable SL_SI91X_ENABLE_NWP_LOGGING in the config_feature_bit_map field of sl_wifi_device_configuration_t when BLE AE is enabled.
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
N/A NWP (Captive Core) logging is not supported for the lite firmware. Do not enable SL_SI91X_ENABLE_NWP_LOGGING in the config_feature_bit_map field of sl_wifi_device_configuration_t. None Do not enable SL_SI91X_ENABLE_NWP_LOGGING in the config_feature_bit_map field of sl_wifi_device_configuration_t.
  • Software variants: Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1606445 SSL Rx throughput may be lower than baseline due to frequent MCS rate dropouts during data transfer (under investigation). None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1638531 When TEXT/DATA are placed in PSRAM, NOLOAD on BSS is ignored, causing BSS to be included in the image and increasing its size. None None
  • Software variants: Standard and Lite
  • OPNs: All SiWx917 PSRAM supported OPNs
  • Boards: BRD4342A
  • Modes: SoC
  • Host interfaces: N/A
N/A LTO is not supported for PSRAM-enabled applications with LLVM or GCC toolchains. None None
  • Software variants: Standard and Lite
  • OPNs: All SiWx917 PSRAM supported OPNs
  • Boards: BRD4342A
  • Modes: SoC
  • Host interfaces: N/A
N/A FreeRTOS tick-less idle mode is currently not supported in the Sensor Hub example application. None None
  • Software variants: Standard and Lite
  • OPNs: All except IC's OPNs
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A UART instances do not support different FIFO thresholds. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1475241 SDC cannot be used with OPAMP as its input. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
N/A The ULP Timer may experience timer drifts due to the inaccuracy of the clock source (RC oscillator). None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1527571 PSRAM can be used for runtime data storage as well as for executing MCU applications. It uses the instruction cache (I-cache) to improve instruction memory access performance. The PSRAM D-cache path is disabled to prevent incorrect data during specific back-to-back accesses. See DCACHE_E301 ERRATA for more details. Refer to the D-Cache Errata. None None
  • Software variants: Standard and Lite
  • OPNs: All SiWx917 PSRAM supported OPNs
  • Boards: BRD4342A
  • Modes: SoC
  • Host interfaces: N/A
N/A Peripheral clock sources are currently fixed and cannot be configured by the user. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
N/A GPDMA driver currently supports only memory-to-memory transfers. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
N/A I2C receive operations using DMA may fail because the IC DATA CMD register must be programmed with a read command for each byte. Using two DMA channels (for programming the register and for data transfer) can lead to synchronization issues due to DMA flow control delays. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1567865 SSI Dual and Quad mode supports address lengths up to 32 bits only. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
N/A The DMA controller does not support timeout or threshold interrupts for half-full or full states. For asynchronous transactions, the application must implement handshaking mechanisms to ensure proper synchronization and data transfer control. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
N/A Only a few wakeup sources (ULP GPIO, ULP Timer, ULP ADC, ULP Comparator, and ULP UART) are currently supported for the PS1 state in the Power Manager. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1648684 SSL Tx/Rx throughput drop is observed in coex mode. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1656537 WPA3 Wi-Fi reconnect fails with sl_wifi_connect() timeout (error 0x00000007). None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1676598 UART RS485 baremetal and FreeRTOS applications do not work as expected on the 4342A PSRAM board. None None
  • Software variants: Standard and Lite
  • OPNs: All SiWx917 PSRAM supported OPNs
  • Boards: BRD4342A
  • Modes: SoC
  • Host interfaces: N/A
1623025 ULP SSI Master supports only CS1 due to hardware limitations on the BRD4343C board. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: BRD4343C
  • Modes: SoC
  • Host interfaces: N/A