Structure for setting SMP pairing capability data.
Public Attributes#
Device input output capability
0x00 - Display Only
0x01 - Display Yes/No
0x02 - Keyboard Only
0x03 - No Input No Output 0x04 - Keyboard Display.
oob_data_flag
0 - disable
Authentication Request contains bonding type
MITM Request - BIT(2)
Secure Connections - BIT(3)
Keypress - BIT(4)
CT2 - BIT(5)
Supported Encryption key size 7 to 16 bytes.
Initiator generates/requires the no .of keys after successful paring
BIT(0) - EncKey: Initiator distributes the LTK followed by EDIV and Rand
BIT(1) - IdKey : Initiator distributes the IRK followed by its address
BIT(2) - Sign : Initiator distributes the CSRK
BIT(3) - BIT(7): Reserved for future use.
Responder generates/requires the no .of keys after successful paring
BIT(0) - EncKey: Responder distributes the LTK followed by EDIV and Rand
BIT(1) - IdKey : Responder distributes the IRK followed by its address
BIT(2) - Sign : Responder distributes the CSRK
BIT(3) - BIT(7): Reserved for future use.
Public Attribute Documentation#
io_capability#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::io_capability
Device input output capability
0x00 - Display Only
0x01 - Display Yes/No
0x02 - Keyboard Only
0x03 - No Input No Output 0x04 - Keyboard Display.
1277
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
oob_data_flag#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::oob_data_flag
oob_data_flag
0 - disable
1 - enable
1282
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
auth_req#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::auth_req
Authentication Request contains bonding type
MITM Request - BIT(2)
Secure Connections - BIT(3)
Keypress - BIT(4)
CT2 - BIT(5)
1292
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
enc_key_size#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::enc_key_size
Supported Encryption key size 7 to 16 bytes.
1294
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
ini_key_distribution#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::ini_key_distribution
Initiator generates/requires the no .of keys after successful paring
BIT(0) - EncKey: Initiator distributes the LTK followed by EDIV and Rand
BIT(1) - IdKey : Initiator distributes the IRK followed by its address
BIT(2) - Sign : Initiator distributes the CSRK
BIT(3) - BIT(7): Reserved for future use.
1304
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
rsp_key_distribution#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::rsp_key_distribution
Responder generates/requires the no .of keys after successful paring
BIT(0) - EncKey: Responder distributes the LTK followed by EDIV and Rand
BIT(1) - IdKey : Responder distributes the IRK followed by its address
BIT(2) - Sign : Responder distributes the CSRK
BIT(3) - BIT(7): Reserved for future use.
1314
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h