Structure representing the parameters of a remote connection parameter request event in BLE.

Public Attributes#

uint8_t

Device address of the remote device.

uint16_t

Minimum connection interval.

uint16_t

Maximum connection interval.

uint16_t

Slave Latency.

uint16_t

Supervision Timeout.

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_event_remote_conn_param_req_s::dev_addr[6]

Device address of the remote device.


conn_interval_min#

uint16_t rsi_ble_event_remote_conn_param_req_s::conn_interval_min

Minimum connection interval.


conn_interval_max#

uint16_t rsi_ble_event_remote_conn_param_req_s::conn_interval_max

Maximum connection interval.


conn_latency#

uint16_t rsi_ble_event_remote_conn_param_req_s::conn_latency

Slave Latency.


timeout#

uint16_t rsi_ble_event_remote_conn_param_req_s::timeout

Supervision Timeout.