ae periodic adv report event

Public Attributes#

uint16_t

uint16_t Sync_Handle, It identifies the periodic Advertising train.

int8_t

int8_t TX_Power, It shall be set based on the AUX_SYNC_IND PDU TX_Power ranges from -127 to +20 and it's units is in dBm

int8_t

int8_t RSSI , this parameter contains the RSSI value, excluding any constant tone Extension.

uint8_t

Unused byte for alignment.

uint8_t

uint8_t Data_Status, It specifies about the status of the data sent 0x00 - Data Complete 0x01 - Data Incomplete, more Data to come

uint8_t

uint8_t Data_Length ,Length of the Data Field, Ranges from 0 to 247

uint8_t

uint8[256] Data, Data received from a Periodic Advertising Packet

Public Attribute Documentation#

sync_handle#

uint16_t rsi_ble_per_adv_report_s::sync_handle

uint16_t Sync_Handle, It identifies the periodic Advertising train.

Range : 0x0000 to 0x0EFF


tx_power#

int8_t rsi_ble_per_adv_report_s::tx_power

int8_t TX_Power, It shall be set based on the AUX_SYNC_IND PDU TX_Power ranges from -127 to +20 and it's units is in dBm


RSSI#

int8_t rsi_ble_per_adv_report_s::RSSI

int8_t RSSI , this parameter contains the RSSI value, excluding any constant tone Extension.

RSSI ranges from -127 to +20 and it's units is in dBm


unused#

uint8_t rsi_ble_per_adv_report_s::unused

Unused byte for alignment.


data_status#

uint8_t rsi_ble_per_adv_report_s::data_status

uint8_t Data_Status, It specifies about the status of the data sent 0x00 - Data Complete 0x01 - Data Incomplete, more Data to come


data_len#

uint8_t rsi_ble_per_adv_report_s::data_len

uint8_t Data_Length ,Length of the Data Field, Ranges from 0 to 247


data#

uint8_t rsi_ble_per_adv_report_s::data[ADV_DATA_LEN]

uint8[256] Data, Data received from a Periodic Advertising Packet