ae adv set terminated report event

Public Attributes#

uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

status#

uint8_t rsi_ble_adv_set_terminated_s::status

uint8_t status : Status shows the status on how the Advertising ended 0 - Advertising successfully ended with a connection being created !0 - Advertising ended for another reason and usually error codes would be listed


Definition at line 1869 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

adv_handle#

uint8_t rsi_ble_adv_set_terminated_s::adv_handle

uint8_t Advertising_Handle : Advertising_Handle in which Advertising has ended, Range : 0x00 to 0xEF


Definition at line 1871 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

conn_handle#

uint16_t rsi_ble_adv_set_terminated_s::conn_handle

uint16_t Connection_Handle : It is the Connection Handle of the connection whose creation ended the advertising, Range : 0x00 to 0xEF


Definition at line 1873 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

num_completed_ae_events#

uint8_t rsi_ble_adv_set_terminated_s::num_completed_ae_events

uint8_t Num_Completed_Extended_Advertising_Events Number of completed extended advertising events transmitted by the Controller


Definition at line 1878 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h