Structure indicates the received write information from the remote device.

Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_event_write_s::dev_addr[RSI_DEV_ADDR_LEN]

remote device address


Definition at line 1032 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

reserved#

uint8_t rsi_ble_event_write_s::reserved

Reserved for future use


Definition at line 1034 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

pkt_type#

uint8_t rsi_ble_event_write_s::pkt_type

Type of the event received from the remote device

  • RSI_BLE_WRITE_CMD_EVENT 0x01

  • RSI_BLE_WRITE_REQUEST_EVENT 0x02

  • RSI_BLE_NOTIFICATION_EVENT 0x03

  • RSI_BLE_INDICATION_EVENT 0x04


Definition at line 1058 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

handle#

uint8_t rsi_ble_event_write_s::handle[2]

attribute handle


Definition at line 1060 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

length#

uint8_t rsi_ble_event_write_s::length

length of attribute value


Definition at line 1062 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

att_value#

uint8_t rsi_ble_event_write_s::att_value[RSI_DEV_ATT_LEN]

This contains the attribute value. The maximum value is 240, refer to RSI_DEV_ATT_LEN Macro


Definition at line 1064 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h