Structure representing the data for the length update event.

Public Attributes#

uint8_t
uint16_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_event_data_length_update_s::dev_addr[RSI_DEV_ADDR_LEN]

Device address of the remote device.


Definition at line 482 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

MaxTxOctets#

uint16_t rsi_ble_event_data_length_update_s::MaxTxOctets

Maximum TX Octets to be transmitted


Definition at line 484 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

MaxTxTime#

uint16_t rsi_ble_event_data_length_update_s::MaxTxTime

Maximum TX time to transmit the MaxTxOctets


Definition at line 486 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

MaxRxOctets#

uint16_t rsi_ble_event_data_length_update_s::MaxRxOctets

Maximum Rx Octets to be received


Definition at line 488 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

MaxRxTime#

uint16_t rsi_ble_event_data_length_update_s::MaxRxTime

Maximum Rx time to receive the MaxRxOctets


Definition at line 490 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h