Structure representing the BLE read request.
This structure is used to define the parameters for a BLE read request, including the remote device address, attribute handle, request type, and offset.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_read_req_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address
Definition at line
1108
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
handle#
uint16_t rsi_ble_read_req_s::handle
Attribute handle
Definition at line
1110
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
type#
uint8_t rsi_ble_read_req_s::type
Request type: 0 - Read request, 1 - Read Blob request
Definition at line
1112
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
reserved#
uint8_t rsi_ble_read_req_s::reserved
Reserved for future use
Definition at line
1114
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
offset#
uint16_t rsi_ble_read_req_s::offset
Offset of attribute value to be read
Definition at line
1116
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h