Structure representing the CBFC connection complete event.
This structure is used to define the parameters for a BLE event that indicates the completion of a Circular Buffer Flow Control (CBFC) connection with a remote device.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_event_cbfc_conn_complete_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the remote device
Definition at line
1199
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
psm#
uint16_t rsi_ble_event_cbfc_conn_complete_s::psm
Protocol/Service Multiplexer (PSM) value
Definition at line
1201
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
mtu#
uint16_t rsi_ble_event_cbfc_conn_complete_s::mtu
Maximum Transmission Unit (MTU) size
Definition at line
1203
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
mps#
uint16_t rsi_ble_event_cbfc_conn_complete_s::mps
Maximum PDU Size (MPS)
Definition at line
1205
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
lcid#
uint16_t rsi_ble_event_cbfc_conn_complete_s::lcid
Local Channel Identifier (LCID)
Definition at line
1207
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h