ae adv report event

Public Attributes#

uint16_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

event_type#

uint16_t rsi_ble_ae_adv_report_s::event_type

Bit Number

Parameter Description

0

Connectable Advertising

1

Scannable Advertising

2

Direct Advertising

3

Scan Response

4

Legacy Advertising PDUs used

5 to 6

Data status :

| | | 0b00 = complete | | | 0b01 = Incomplete, more data to come | | | 0b10 = Incomplete, data truncated, no more to come | | | 0b11 = Reserved for future use |


Definition at line 1716 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

remote_addr_type#

uint8_t rsi_ble_ae_adv_report_s::remote_addr_type

uint8_t Remote Address Type, Indicates the type of the Address 0x00 - Public Device Address 0x01 - Random Device Address 0x02 - Public Identity Address (corresponds to Resolved Private Address) 0x03 - Random (static) Identity Address (corresponds to Resolved Private Address)


Definition at line 1724 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

remote_addr#

uint8_t rsi_ble_ae_adv_report_s::remote_addr[DEVICE_ADDR_LEN]

uint8[6] remote_Address : Address of the remote address Type


Definition at line 1726 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

pri_phy#

uint8_t rsi_ble_ae_adv_report_s::pri_phy

uint8_t Primary PHY 0x01 - Advertiser PHY is LE 1M 0x03 - Advertiser PHY is LE Coded


Definition at line 1732 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

sec_phy#

uint8_t rsi_ble_ae_adv_report_s::sec_phy

uint8_t Secondary PHY 0x00 - No packets on the secondary advertising physical channel 0x01 - Advertiser PHY is LE 1M 0x02 - Advertiser PHY is LE 2M 0x03 - Advertiser PHY is LE Coded


Definition at line 1740 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

SID#

uint8_t rsi_ble_ae_adv_report_s::SID

uint8_t Advertising_SID#

Value

Parameter Description

0x00 to 0x0F

Value of the Advertising SID subfield in the ADI field of the PDU or,

for scan responses, in the ADI field of the original scannable advertisement | | 0xFF | No ADI field provided |


Definition at line 1750 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

tx_power#

uint8_t rsi_ble_ae_adv_report_s::tx_power

uint8_t TX_Power, It shall be set based on the AUX_SYNC_IND PDU TX_Power ranges from -127 to +20 and it's units is in dBm


Definition at line 1755 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

RSSI#

uint8_t rsi_ble_ae_adv_report_s::RSSI

uint8_t RSSI , this parameter contains the RSSI value, excluding any constant tone Extension. RSSI ranges from -127 to +20 and it's units is in dBm


Definition at line 1760 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

per_adv_interval#

uint16_t rsi_ble_ae_adv_report_s::per_adv_interval

uint16_t Periodic_Advertising_Interval. This parameter specifies the interval between the periodic advertising events


Definition at line 1762 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

direct_addr_type#

uint8_t rsi_ble_ae_adv_report_s::direct_addr_type

uint8_t Direct Address Type ,Indicates the type of the Address 0x00 - Public Device Address 0x01 - Random Device Address 0x02 - Public Identity Address (corresponds to Resolved Private Address) 0x03 - Random (static) Identity Address (corresponds to Resolved Private Address) 0xFE - Resolves Private Address


Definition at line 1771 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

direct_addr#

uint8_t rsi_ble_ae_adv_report_s::direct_addr[DEVICE_ADDR_LEN]

uint8[6] Direct_Address, Direct_Address of the Advertiser type


Definition at line 1773 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

data_len#

uint8_t rsi_ble_ae_adv_report_s::data_len

uint8_t Data _length , Length of the Data field for each device which responded , ranges from 0 to 229


Definition at line 1775 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

data#

uint8_t rsi_ble_ae_adv_report_s::data[ADV_DATA_LEN]

uint8[256] Data


Definition at line 1777 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h