Structure represents the remote device information event.

This structure is used to define the parameters for a BLE event that provides information about a remote device.

Public Attributes#

uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_event_remote_device_info_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address


Definition at line 1005 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

remote_version#

uint8_t rsi_ble_event_remote_device_info_s::remote_version

Remote device version


Definition at line 1007 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

remote_company_id#

uint16_t rsi_ble_event_remote_device_info_s::remote_company_id

Remote device company ID


Definition at line 1009 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

remote_sub_version#

uint16_t rsi_ble_event_remote_device_info_s::remote_sub_version

Remote device sub-version


Definition at line 1011 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h