The structure represents the parameters of a remote connection parameter request event.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_event_remote_conn_param_req_s::dev_addr[6]
Device address of the remote device
Definition at line
441
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
conn_interval_min#
uint16_t rsi_ble_event_remote_conn_param_req_s::conn_interval_min
Minimum connection interval
Definition at line
443
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
conn_interval_max#
uint16_t rsi_ble_event_remote_conn_param_req_s::conn_interval_max
Maximum connection interval
Definition at line
445
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
conn_latency#
uint16_t rsi_ble_event_remote_conn_param_req_s::conn_latency
Slave Latency
Definition at line
447
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
timeout#
uint16_t rsi_ble_event_remote_conn_param_req_s::timeout
Supervision Timeout
Definition at line
449
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h