Structure to hold the event data for encryption enabled event.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_bt_event_encryption_enabled_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device Address
Definition at line
226
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
enabled#
uint8_t rsi_bt_event_encryption_enabled_s::enabled
Status of the Encryption
ENCRYPT_ENABLED BIT(0) --> To indicate or set encryption is enabled AUTH_LTK_OR_STK_ENC
BIT(1) --> To indicate or set Authenticated Pairing and Encryption UN_AUTH_LTK_OR_STK_ENC
BIT(2) --> To indicate or set UnAuthenticated Pairing and Encryption AUTH_LTK_WITH_LE_SC_ENC
BIT(3) --> To indicate or set Authenticated Pairing and Encryption with LE SC
Definition at line
236
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
sc_enable#
uint8_t rsi_bt_event_encryption_enabled_s::sc_enable
BLE Secure Connections Enable/Disable indication
0 --> Disable
1 --> Enable
Definition at line
242
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
localediv#
uint16_t rsi_bt_event_encryption_enabled_s::localediv
Local device EDIV
Definition at line
244
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
localrand#
uint8_t rsi_bt_event_encryption_enabled_s::localrand[8]
Local RAND
Definition at line
246
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
localltk#
uint8_t rsi_bt_event_encryption_enabled_s::localltk[16]
Local Long term Key
Definition at line
248
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
dev_addr_type#
uint8_t rsi_bt_event_encryption_enabled_s::dev_addr_type
Remote Device Address type
Definition at line
250
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h