Public Attributes#
void(*
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
Routing slave to recieve route.
uint8_t
Destination of route (if 0 destination will be self). Destination can be a SUC.
uint8_t
Route to be assigned as priority route - set to zeroes to NOT supply a priority route (recommended)
uint8_t
Public Attribute Documentation#
Handle#
void(* SAssignReturnRoute::Handle) (void)
Definition at line
1430
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
ReturnRouteReceiverNodeId#
node_id_t SAssignReturnRoute::ReturnRouteReceiverNodeId
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
Definition at line
1434
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
RouteDestinationNodeId#
node_id_t SAssignReturnRoute::RouteDestinationNodeId
Routing slave to recieve route.
Definition at line
1435
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
aPriorityRouteRepeaters#
uint8_t SAssignReturnRoute::aPriorityRouteRepeaters[4]
Destination of route (if 0 destination will be self). Destination can be a SUC.
Definition at line
1436
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
PriorityRouteSpeed#
uint8_t SAssignReturnRoute::PriorityRouteSpeed
Route to be assigned as priority route - set to zeroes to NOT supply a priority route (recommended)
Definition at line
1437
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
isSucRoute#
uint8_t SAssignReturnRoute::isSucRoute
Definition at line
1438
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h