Public Attributes#

void(*

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.

bool

Node to have its return routes deleted..

Public Attribute Documentation#

Handle#

void(* SDeleteReturnRoute::Handle) (void)

Definition at line 1449 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

DestNodeId#

node_id_t SDeleteReturnRoute::DestNodeId

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.


Definition at line 1453 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

bDeleteSuc#

bool SDeleteReturnRoute::bDeleteSuc

Node to have its return routes deleted..


Definition at line 1454 of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h