Macros |
|
| #define | NUM_ADC_USERS 3U |
|
Be sure to update
NUM_ADC_USERS
if additional users are added to the
ADCUser
list.
|
|
| #define | ADC_MUXN_BITS (4) |
| #define | ADC_MUX_ADC0 0x0 |
| #define | ADC_MUX_ADC1 0x1 |
| #define | ADC_MUX_ADC2 0x2 |
| #define | ADC_MUX_ADC3 0x3 |
| #define | ADC_MUX_ADC4 0x4 |
| #define | ADC_MUX_ADC5 0x5 |
| #define | ADC_MUX_GND 0x8 |
| #define | ADC_MUX_VREF2 0x9 |
| #define | ADC_MUX_VREF 0xA |
| #define | ADC_MUX_VREG2 0xB |
Typedefs |
|
| typedef uint8_t | ADCChannelType |
|
A type for the channel enumeration.
|
|
| typedef uint8_t | ADCReferenceType |
|
A type for the reference voltage enumeration.
|
|
| typedef uint8_t | ADCRateType |
|
A type for the sample rate enumeration.
|
|
Enumerations |
|
| enum |
ADCUser
{
ADC_USER_LQI = 0, ADC_USER_APP = 1, ADC_USER_APP2 = 2 } |
|
ADC functions employ a user ID to keep different users separate.
|
|
| enum | { ADC_REF_INT = 42U } |
|
ADCReferenceType Enumeration. Note: EM35x only supports one reference type: Internal.
|
|
| enum |
{
ADC_SAMPLE_CLOCKS_32 = 0x0, ADC_SAMPLE_CLOCKS_64 = 0x1, ADC_SAMPLE_CLOCKS_128 = 0x2, ADC_SAMPLE_CLOCKS_256 = 0x3, ADC_SAMPLE_CLOCKS_512 = 0x4, ADC_SAMPLE_CLOCKS_1024 = 0x5, ADC_SAMPLE_CLOCKS_2048 = 0x6, ADC_SAMPLE_CLOCKS_4096 = 0x7 } |
|
ADCRateType enumeration. These rates are specified in the number of clock cycles That a conversion takes. The actual time taken will depend on the selected ADC clock rate. (Default is 6MHz)
|
|
| enum |
{
ADC_CONVERSION_TIME_US_32 = 0x0, ADC_CONVERSION_TIME_US_64 = 0x1, ADC_CONVERSION_TIME_US_128 = 0x2, ADC_CONVERSION_TIME_US_256 = 0x3, ADC_CONVERSION_TIME_US_512 = 0x4, ADC_CONVERSION_TIME_US_1024 = 0x5, ADC_CONVERSION_TIME_US_2048 = 0x6, ADC_CONVERSION_TIME_US_4096 = 0x7 } |
|
ADC rates for compatibility with EM2xx applications. For EM35x only applications, the ADC_SAMPLE_CLOCKS_nnn definitions should be used instead.
|
|
| enum |
{
ADC_SOURCE_ADC0_VREF2 = ((ADC_MUX_ADC0 << ADC_MUXN_BITS) + ADC_MUX_VREF2), ADC_SOURCE_ADC0_GND = ((ADC_MUX_ADC0 << ADC_MUXN_BITS) + ADC_MUX_GND), ADC_SOURCE_ADC1_VREF2 = ((ADC_MUX_ADC1 << ADC_MUXN_BITS) + ADC_MUX_VREF2), ADC_SOURCE_ADC1_GND = ((ADC_MUX_ADC1 << ADC_MUXN_BITS) + ADC_MUX_GND), ADC_SOURCE_ADC2_VREF2 = ((ADC_MUX_ADC2 << ADC_MUXN_BITS) + ADC_MUX_VREF2), ADC_SOURCE_ADC2_GND = ((ADC_MUX_ADC2 << ADC_MUXN_BITS) + ADC_MUX_GND), ADC_SOURCE_ADC3_VREF2 = ((ADC_MUX_ADC3 << ADC_MUXN_BITS) + ADC_MUX_VREF2), ADC_SOURCE_ADC3_GND = ((ADC_MUX_ADC3 << ADC_MUXN_BITS) + ADC_MUX_GND), ADC_SOURCE_ADC4_VREF2 = ((ADC_MUX_ADC4 << ADC_MUXN_BITS) + ADC_MUX_VREF2), ADC_SOURCE_ADC4_GND = ((ADC_MUX_ADC4 << ADC_MUXN_BITS) + ADC_MUX_GND), ADC_SOURCE_ADC5_VREF2 = ((ADC_MUX_ADC5 << ADC_MUXN_BITS) + ADC_MUX_VREF2), ADC_SOURCE_ADC5_GND = ((ADC_MUX_ADC5 << ADC_MUXN_BITS) + ADC_MUX_GND), ADC_SOURCE_ADC1_ADC0 = ((ADC_MUX_ADC1 << ADC_MUXN_BITS) + ADC_MUX_ADC0), ADC_SOURCE_ADC0_ADC1 = ((ADC_MUX_ADC1 << ADC_MUXN_BITS) + ADC_MUX_ADC0), ADC_SOURCE_ADC3_ADC2 = ((ADC_MUX_ADC3 << ADC_MUXN_BITS) + ADC_MUX_ADC2), ADC_SOURCE_ADC2_ADC3 = ((ADC_MUX_ADC3 << ADC_MUXN_BITS) + ADC_MUX_ADC2), ADC_SOURCE_ADC5_ADC4 = ((ADC_MUX_ADC5 << ADC_MUXN_BITS) + ADC_MUX_ADC4), ADC_SOURCE_GND_VREF2 = ((ADC_MUX_GND << ADC_MUXN_BITS) + ADC_MUX_VREF2), ADC_SOURCE_VGND = ((ADC_MUX_GND << ADC_MUXN_BITS) + ADC_MUX_GND), ADC_SOURCE_VREF_VREF2 = ((ADC_MUX_VREF << ADC_MUXN_BITS) + ADC_MUX_VREF2), ADC_SOURCE_VREF = ((ADC_MUX_VREF << ADC_MUXN_BITS) + ADC_MUX_GND), ADC_SOURCE_VREG2_VREF2 = ((ADC_MUX_VREG2 << ADC_MUXN_BITS) + ADC_MUX_VREF2), ADC_SOURCE_VDD_GND = ((ADC_MUX_VREG2 << ADC_MUXN_BITS) + ADC_MUX_GND) } |
Functions |
|
| void | halInternalInitAdc (void) |
|
Initializes and powers-up the ADC. Should also be called to wake from sleep. The ADC is required for EM250 stack operation so this function must be called from halInit.
|
|
| void | halInternalSleepAdc (void) |
|
Shuts down the voltage reference and ADC system to minimize power consumption in sleep.
|
|
| EmberStatus | halStartAdcConversion ( ADCUser id, ADCReferenceType reference, ADCChannelType channel, ADCRateType rate) |
Starts an ADC conversion for the user specified by
id
.
|
|
| EmberStatus | halRequestAdcData ( ADCUser id, uint16_t *value) |
Returns the status of a pending conversion previously started by
halStartAdcConversion()
. If the conversion is complete, writes the raw register value of the conversion (the unaltered value taken directly from the ADC's data register) into
value
.
|
|
| EmberStatus | halReadAdcBlocking ( ADCUser id, uint16_t *value) |
Waits for the user's request to complete and then, if a conversion was done, writes the raw register value of the conversion (the unaltered value taken directly from the ADC's data register) into
value
and returns
EMBER_ADC_CONVERSION_DONE
, or immediately returns
EMBER_ADC_NO_CONVERSION_PENDING
.
|
|
| EmberStatus | halAdcCalibrate ( ADCUser id) |
|
Calibrates or recalibrates the ADC system.
|
|
| int32_t | halConvertValueToVolts (uint16_t value) |
|
Convert the raw register value (the unaltered value taken directly from the ADC's data register) into a signed fixed point value with units 10^-4 Volts. The returned value will be in the range -12000 to +12000 (-1.2000 volts to +1.2000 volts).
|
|
| void | emberCalibrateVref (void) |
|
Calibrates Vref to be 1.2V +/-10mV.
|
|
| void | halAdcSetClock (bool slow) |
|
Set ADC clock mode.
|
|
| bool | halAdcGetClock (void) |
|
Get ADC clock mode.
|
|
| uint16_t | halMeasureVdd ( ADCRateType rate) |
|
Measures VDD_PADS in millivolts at the specified sample rate Due to the conversions performed, this function takes slightly under 250us with a variation across successive conversions approximately +/-20mv of the average conversion.
|
|
Detailed Description
Sample A/D converter driver.
See
adc.h
for source code.
- Note
- The EmberZNet stack does use these functions.
To use the ADC system, include this file and ensure that halInternalInitAdc() is called whenever the microcontroller is started. Call halInternalSleepAdc() to sleep the module and halInternalInitAdc() to wake up the module.
A "user" is a separate thread of execution and usage. That is, internal Ember code is one user and clients are a different user. But a client that is calling the ADC in two different functions constitutes only one user, as long as the ADC access is not interleaved.
- Note
- This code does not allow access to the continuous reading mode of the ADC, which some clients may require.
Many functions in this file return an
EmberStatus
value. See
error-def.h
for definitions of all
EmberStatus
return values.
Sample A/D converter driver.
- Note
- EM35x ADC driver support is preliminary and may be changed in a future release
Macro Definition Documentation
| #define ADC_MUX_ADC0 0x0 |
Channel 0 : ADC0 on PB5
| #define ADC_MUX_ADC1 0x1 |
Channel 1 : ADC0 on PB6
| #define ADC_MUX_ADC2 0x2 |
Channel 2 : ADC0 on PB7
| #define ADC_MUX_ADC3 0x3 |
Channel 3 : ADC0 on PC1
| #define ADC_MUX_ADC4 0x4 |
Channel 4 : ADC0 on PA4
| #define ADC_MUX_ADC5 0x5 |
Channel 5 : ADC0 on PA5
| #define ADC_MUX_GND 0x8 |
Channel 8 : VSS (0V) - not for high voltage range
| #define ADC_MUX_VREF 0xA |
Channel A : VREF (1.2V)
| #define ADC_MUX_VREF2 0x9 |
Channel 9 : VREF/2 (0.6V)
| #define ADC_MUX_VREG2 0xB |
Channel B : Regulator/2 (0.9V) - not for high voltage range
| #define ADC_MUXN_BITS (4) |
| #define NUM_ADC_USERS 3U |
Be sure to update NUM_ADC_USERS if additional users are added to the ADCUser list.
Typedef Documentation
| typedef uint8_t ADCChannelType |
A type for the channel enumeration.
| typedef uint8_t ADCRateType |
A type for the sample rate enumeration.
| typedef uint8_t ADCReferenceType |
A type for the reference voltage enumeration.
Enumeration Type Documentation
| anonymous enum |
| anonymous enum |
ADCRateType enumeration. These rates are specified in the number of clock cycles That a conversion takes. The actual time taken will depend on the selected ADC clock rate. (Default is 6MHz)
| anonymous enum |
ADC rates for compatibility with EM2xx applications. For EM35x only applications, the ADC_SAMPLE_CLOCKS_nnn definitions should be used instead.
| anonymous enum |
| enum ADCUser |
ADC functions employ a user ID to keep different users separate.
Avoid many users because each user requires some amount of state storage.
- See also
- NUM_ADC_USERS
| Enumerator | |
|---|---|
| ADC_USER_LQI |
LQI User ID. |
| ADC_USER_APP |
Application User ID |
| ADC_USER_APP2 |
Application User ID |
Function Documentation
| void emberCalibrateVref | ( | void |
|
) |
Calibrates Vref to be 1.2V +/-10mV.
This function must be called from halInternalInitAdc() before making ADC readings. This function is not intended to be called from any function other than halInternalInitAdc() . This function ensures that the master cell voltage and current bias values are calibrated before calibrating Vref.
| EmberStatus halAdcCalibrate | ( | ADCUser |
id
|
) |
Calibrates or recalibrates the ADC system.
Use this function to (re)calibrate as needed. This function is intended for the EM250 microcontroller, which requires proper calibration to calculate a human readible value (a value in volts). If the app does not call this function, the first time (and only the first time) the function halConvertValueToVolts() is called, this function is invoked. To maintain accurate volt calculations, the application should call this whenever it expects the temperature of the micro to change.
- Parameters
-
idAn ADC user.
- Returns
-
One of the following:
- EMBER_ADC_CONVERSION_DONE if the calibration is complete.
- EMBER_ERR_FATAL if the calibration failed.
| bool halAdcGetClock | ( | void |
|
) |
Get ADC clock mode.
- Returns
- A true if the slow clock is selected.
| void halAdcSetClock | ( | bool |
slow
|
) |
Set ADC clock mode.
- Parameters
-
slowA bool to select slow or normal clock.
| int32_t halConvertValueToVolts | ( | uint16_t |
value
|
) |
Convert the raw register value (the unaltered value taken directly from the ADC's data register) into a signed fixed point value with units 10^-4 Volts. The returned value will be in the range -12000 to +12000 (-1.2000 volts to +1.2000 volts).
Use this function to get a human useful value.
- Parameters
-
valueAn uint16_t to be converted.
- Returns
- Volts as signed fixed point with units 10^-4 Volts.
| void halInternalInitAdc | ( | void |
|
) |
Initializes and powers-up the ADC. Should also be called to wake from sleep. The ADC is required for EM250 stack operation so this function must be called from halInit.
| void halInternalSleepAdc | ( | void |
|
) |
Shuts down the voltage reference and ADC system to minimize power consumption in sleep.
| uint16_t halMeasureVdd | ( | ADCRateType |
rate
|
) |
Measures VDD_PADS in millivolts at the specified sample rate Due to the conversions performed, this function takes slightly under 250us with a variation across successive conversions approximately +/-20mv of the average conversion.
- Returns
- A measurement of VDD_PADS in millivolts.
| EmberStatus halReadAdcBlocking | ( | ADCUser |
id,
|
| uint16_t * |
value
|
||
| ) |
Waits for the user's request to complete and then, if a conversion was done, writes the raw register value of the conversion (the unaltered value taken directly from the ADC's data register) into
value
and returns
EMBER_ADC_CONVERSION_DONE
, or immediately returns
EMBER_ADC_NO_CONVERSION_PENDING
.
- Parameters
-
idAn ADC user. valuePointer to an uint16_t to be loaded with the new value. Take note that the Atmel's ADC only generates 8-bit values which are loaded into the lower 8 bits of value.
- Returns
-
One of the following:
- EMBER_ADC_CONVERSION_DONE if the conversion is complete.
-
EMBER_ADC_NO_CONVERSION_PENDING
if
iddoes not have a pending conversion.
| EmberStatus halRequestAdcData | ( | ADCUser |
id,
|
| uint16_t * |
value
|
||
| ) |
Returns the status of a pending conversion previously started by
halStartAdcConversion()
. If the conversion is complete, writes the raw register value of the conversion (the unaltered value taken directly from the ADC's data register) into
value
.
- Parameters
-
idAn ADC user. valuePointer to an uint16_t to be loaded with the new value. Take note that the Atmel's ADC only generates 8-bit values which are loaded into the lower 8 bits of value.
- Returns
-
One of the following:
- EMBER_ADC_CONVERSION_DONE if the conversion is complete.
- EMBER_ADC_CONVERSION_DEFERRED if the conversion is still waiting to start.
- EMBER_ADC_CONVERSION_BUSY if the conversion is currently taking place.
-
EMBER_ADC_NO_CONVERSION_PENDING
if
iddoes not have a pending conversion.
| EmberStatus halStartAdcConversion | ( | ADCUser |
id,
|
| ADCReferenceType |
reference,
|
||
| ADCChannelType |
channel,
|
||
| ADCRateType |
rate
|
||
| ) |
Starts an ADC conversion for the user specified by
id
.
The application must set
reference
to the voltage reference desired (see the ADC references enum, fixed at
ADC_REF_INT
for the em250), set
channel
to the channel number required (see the ADC channel enum), and set
rate
to reflect the number of bits of accuracy desired (see the ADC rates enum, fixed at
ADC_CONVERSION_TIME_US_256
for the Atmega).
- Parameters
-
idAn ADC user. referenceVoltage reference to use, chosen from enum ADCReferenceType (fixed at ADC_REF_INT for the EM250). channelMicroprocessor channel number. For EM250 channels, see the EM250 ADC channels enum. For basic, single-ended Atmel channels, see the Atmega single-ended ADC channels enum. For more complex measurements on Atmels (differential and amped channel numbers), see the Atmel datasheet for your micro. rateEM250 rate number (see the ADC EM250 rate enum).
- Returns
-
One of the following:
- EMBER_ADC_CONVERSION_DEFERRED if the conversion is still waiting to start.
- EMBER_ADC_CONVERSION_BUSY if the conversion is currently taking place.
- EMBER_ERR_FATAL if a passed parameter is invalid.