EmberTokTypeStackZllData Struct Reference
#include <
zll-types.h
>
Data Fields |
|
| uint32_t | bitmask |
| uint16_t | freeNodeIdMin |
| uint16_t | freeNodeIdMax |
| uint16_t | myGroupIdMin |
| uint16_t | freeGroupIdMin |
| uint16_t | freeGroupIdMax |
| uint8_t | rssiCorrection |
Field Documentation
| uint32_t EmberTokTypeStackZllData::bitmask |
| uint16_t EmberTokTypeStackZllData::freeGroupIdMax |
| uint16_t EmberTokTypeStackZllData::freeGroupIdMin |
| uint16_t EmberTokTypeStackZllData::freeNodeIdMax |
| uint16_t EmberTokTypeStackZllData::freeNodeIdMin |
| uint16_t EmberTokTypeStackZllData::myGroupIdMin |
| uint8_t EmberTokTypeStackZllData::rssiCorrection |
The documentation for this struct was generated from the following file:
-
zll-types.h