EM35x standalone bootloader public definitions.
Required Custom Functions |
|
| void | bootloaderMenu (void) |
|
This function must be implemented, providing a bootloader menu.
|
|
Available Bootloader Library Functions |
|
|
Functions implemented by the bootloader library that may be used by custom functions. |
|
| BL_Status | receiveImage (uint8_t commState) |
|
Puts the bootloader into a mode where it will receive an image. commState indicates whether the image is received via serial (COMM_SERIAL) or over the air (COMM_RADIO)
|
|
| bool | checkDebugMenuOption (uint8_t ch) |
|
A hook to the bootloader library for it to check for extra menu options. Only used for ember internal debug builds, not normally needed.
|
|
| BL_Status | initOtaState (void) |
|
Initialize OTA Bootloader state.
|
|
| BL_Status | checkOtaStart (void) |
|
Check to see if the bootloader has detected an OTA upload start.
|
|
| BL_Status | receiveOtaImage (void) |
|
Puts the bootloader into a mode where it will receive an image over the air. The function
checkOtaStart()
should have been called first and it should have returned with a status of
BL_SUCCESS
before calling this function.
|
|
| bool | paIsPresent (void) |
|
Uses the information in the PHY_CONFIG token to determine if a power amplifier is present in the node design.
|
|
| bool | halCheckIntegrity (void) |
|
Validate application integrity by running AES-MMO hash and comparing to AAT.
|
|
Detailed Description
EM35x standalone bootloader public definitions.
See
standalone-bootloader.h
for source code.
Function Documentation
| void bootloaderMenu | ( | void |
|
) |
This function must be implemented, providing a bootloader menu.
| bool checkDebugMenuOption | ( | uint8_t |
ch
|
) |
A hook to the bootloader library for it to check for extra menu options. Only used for ember internal debug builds, not normally needed.
- Returns
- true if the option was handled, false if not.
| BL_Status checkOtaStart | ( | void |
|
) |
Check to see if the bootloader has detected an OTA upload start.
- Note
- OTA support hooks are subject to change!
- Returns
- BL_Status of the success of the function.
| bool halCheckIntegrity | ( | void |
|
) |
Validate application integrity by running AES-MMO hash and comparing to AAT.
- Returns
- false if fails integrity check, true if pass
| BL_Status initOtaState | ( | void |
|
) |
Initialize OTA Bootloader state.
- Note
- OTA support hooks are subject to change!
- Returns
- BL_Status of the success of the function.
| bool paIsPresent | ( | void |
|
) |
Uses the information in the PHY_CONFIG token to determine if a power amplifier is present in the node design.
- Note
- This function must not be called before emBootloaderRadioBoot().
- Returns
- true if a power amplifier is present, false otherwise.
| BL_Status receiveImage | ( | uint8_t |
commState
|
) |
Puts the bootloader into a mode where it will receive an image. commState indicates whether the image is received via serial (COMM_SERIAL) or over the air (COMM_RADIO)
| BL_Status receiveOtaImage | ( | void |
|
) |
Puts the bootloader into a mode where it will receive an image over the air. The function checkOtaStart() should have been called first and it should have returned with a status of BL_SUCCESS before calling this function.
- Note
- OTA support hooks are subject to change!
- Returns
- BL_Status of the success of the function.