EmberZllDeviceInfoRecord Struct Reference
Information discovered during a ZLL scan about the ZLL device's endpoint information.
#include <
zll-types.h
>
Data Fields |
|
| EmberEUI64 | ieeeAddress |
| uint8_t | endpointId |
| uint16_t | profileId |
| uint16_t | deviceId |
| uint8_t | version |
| uint8_t | groupIdCount |
Information discovered during a ZLL scan about the ZLL device's endpoint information.
Field Documentation
| uint16_t EmberZllDeviceInfoRecord::deviceId |
| uint8_t EmberZllDeviceInfoRecord::endpointId |
| uint8_t EmberZllDeviceInfoRecord::groupIdCount |
| EmberEUI64 EmberZllDeviceInfoRecord::ieeeAddress |
| uint16_t EmberZllDeviceInfoRecord::profileId |
| uint8_t EmberZllDeviceInfoRecord::version |
The documentation for this struct was generated from the following file:
-
zll-types.h