EmberVersion Struct Reference
A version structure containing all version information.
#include <
ember-types.h
>
Data Fields |
|
| uint16_t | build |
| uint8_t | major |
| uint8_t | minor |
| uint8_t | patch |
| uint8_t | special |
| EmberVersionType | type |
A version structure containing all version information.
Field Documentation
| uint16_t EmberVersion::build |
| uint8_t EmberVersion::major |
| uint8_t EmberVersion::minor |
| uint8_t EmberVersion::patch |
| uint8_t EmberVersion::special |
| EmberVersionType EmberVersion::type |
The documentation for this struct was generated from the following file:
-
ember-types.h