Common bootloader interface defines and functions.
Macros |
|
| #define | BOOTLOADER_BASE_TYPE (extendedType) ((uint8_t)(((extendedType) >> 8U) & 0xFFU)) |
|
Macro returning the base type of a bootloader when given an extended type.
|
|
| #define | BOOTLOADER_MAKE_EXTENDED_TYPE (baseType, extendedSpecifier) ((uint16_t)(((uint16_t)baseType) << 8U) | (((uint16_t)extendedSpecifier) & 0xFFU)) |
|
Macro returning the extended type of a bootloader when given a base type and extendedSpecifier.
|
|
| #define | BL_EXT_TYPE_NULL (( BL_TYPE_NULL << 8U) | 0x00U) |
|
Macro defining the extended NULL bootloader type.
|
|
| #define | BL_EXT_TYPE_STANDALONE_UNKNOWN (( BL_TYPE_STANDALONE << 8U) | 0x00U) |
|
Macro defining the extended standalone unknown bootloader type.
|
|
| #define | BL_EXT_TYPE_SERIAL_UART (( BL_TYPE_STANDALONE << 8U) | 0x01U) |
|
Macro defining the extended standalone UART bootloader type.
|
|
| #define | BL_EXT_TYPE_SERIAL_UART_OTA (( BL_TYPE_STANDALONE << 8U) | 0x03U) |
|
Macro defining the extended standalone OTA and UART bootloader type.
|
|
| #define | BL_EXT_TYPE_EZSP_SPI (( BL_TYPE_STANDALONE << 8U) | 0x04U) |
| #define | BL_EXT_TYPE_EZSP_SPI_OTA (( BL_TYPE_STANDALONE << 8U) | 0x06U) |
| #define | BL_EXT_TYPE_SERIAL_USB (( BL_TYPE_STANDALONE << 8U) | 0x07U) |
|
Macro defining the extended standalone USB bootloader type.
|
|
| #define | BL_EXT_TYPE_SERIAL_USB_OTA (( BL_TYPE_STANDALONE << 8U) | 0x08U) |
|
Macro defining the extended standalone OTA and USB bootloader type.
|
|
| #define | BL_EXT_TYPE_APP_UNKNOWN (( BL_TYPE_APPLICATION << 8U) | 0x00U) |
|
Macro defining the extended application unknown bootloader type.
|
|
| #define | BL_EXT_TYPE_APP_SPI (( BL_TYPE_APPLICATION << 8U) | 0x01U) |
|
Macro defining the extended application SPI bootloader type.
|
|
| #define | BL_EXT_TYPE_APP_I2C (( BL_TYPE_APPLICATION << 8U) | 0x02U) |
|
Macro defining the extended application I2C bootloader type.
|
|
| #define | BL_EXT_TYPE_APP_LOCAL_STORAGE (( BL_TYPE_APPLICATION << 8U) | 0x03U) |
|
Macro defining a type for the local storage app bootloader.
|
|
| #define | BOOTLOADER_INVALID_VERSION 0xFFFF |
|
Define an invalid bootloader version.
|
|
| #define | CUSTOMER_APPLICATION_VERSION 0 |
|
Macro defining the customer application version stored in the ApplicationProperties_t struct.
|
|
| #define | CUSTOMER_APPLICATION_CAPABILITIES 0 |
|
Macro defining the customer application capabilities stored in the ApplicationProperties_t struct.
|
|
| #define | CUSTOMER_APPLICATION_PRODUCT_ID { 0 } |
|
Macro defining the customer application product ID stored in the ApplicationProperties_t struct.
|
|
| #define | MPSI_PLUGIN_SUPPORT 0 |
|
Macro defining the support for the MPSI protocol stored in the capabilities field of the ApplicationProperties_t struct.
|
|
| #define | APPLICATION_PROPERTIES_CAPABILITIES_MPSI_SUPPORT_BIT 31 |
|
Macro defining the bit position that corresponds to MPSI support in the capabilities field of the ApplicationProperties_t struct.
|
|
| #define | APPLICATION_PROPERTIES_CAPABILITIES |
|
Macro defining the capabilities that this application has. This value is set in the capabilities field of the ApplicationProperties_t struct.
|
|
Functions |
|
| BlBaseType | halBootloaderGetType (void) |
|
Returns the bootloader base type the application was built for.
|
|
| BlExtendedType | halBootloaderGetInstalledType (void) |
|
Returns the extended bootloader type of the bootloader that is present on the chip.
|
|
| uint16_t | halGetBootloaderVersion (void) |
|
Returns the version of the installed bootloader, regardless of its type.
|
|
| void | halGetExtendedBootloaderVersion (uint32_t * emberVersion , uint32_t *customerVersion) |
|
Return extended bootloader version information, if supported. This API is not supported for EM2XX chips and only returns extra information on bootloaders built on or after the 4.7 release.
|
|
Bootloader Numerical Definitions |
|
|
These are numerical definitions for the possible bootloader types and a typedef of the bootloader base type. |
|
| #define | BL_TYPE_NULL (0) |
|
Numerical definition for a bootloader type.
|
|
| #define | BL_TYPE_STANDALONE (1) |
|
Numerical definition for a bootloader type.
|
|
| #define | BL_TYPE_APPLICATION (2) |
|
Numerical definition for a bootloader type.
|
|
| #define | BL_TYPE_BOOTLOADER (3) |
|
Numerical definition for a bootloader type.
|
|
| #define | BL_TYPE_SMALL_BOOTLOADER (4) |
|
Numerical definition for a bootloader type.
|
|
Bootloader type definitions |
|
| typedef uint8_t | BlBaseType |
|
Define the bootloader base type.
|
|
| typedef uint16_t | BlExtendedType |
|
Define the bootloader extended type.
|
|
Detailed Description
Common bootloader interface defines and functions.
See
bootloader-interface.h
for source code.
Macro Definition Documentation
| #define APPLICATION_PROPERTIES_CAPABILITIES |
Macro defining the capabilities that this application has. This value is set in the capabilities field of the ApplicationProperties_t struct.
| #define APPLICATION_PROPERTIES_CAPABILITIES_MPSI_SUPPORT_BIT 31 |
Macro defining the bit position that corresponds to MPSI support in the capabilities field of the ApplicationProperties_t struct.
| #define BL_EXT_TYPE_APP_I2C (( BL_TYPE_APPLICATION << 8U) | 0x02U) |
Macro defining the extended application I2C bootloader type.
| #define BL_EXT_TYPE_APP_LOCAL_STORAGE (( BL_TYPE_APPLICATION << 8U) | 0x03U) |
Macro defining a type for the local storage app bootloader.
| #define BL_EXT_TYPE_APP_SPI (( BL_TYPE_APPLICATION << 8U) | 0x01U) |
Macro defining the extended application SPI bootloader type.
| #define BL_EXT_TYPE_APP_UNKNOWN (( BL_TYPE_APPLICATION << 8U) | 0x00U) |
Macro defining the extended application unknown bootloader type.
| #define BL_EXT_TYPE_EZSP_SPI (( BL_TYPE_STANDALONE << 8U) | 0x04U) |
| #define BL_EXT_TYPE_EZSP_SPI_OTA (( BL_TYPE_STANDALONE << 8U) | 0x06U) |
| #define BL_EXT_TYPE_NULL (( BL_TYPE_NULL << 8U) | 0x00U) |
Macro defining the extended NULL bootloader type.
| #define BL_EXT_TYPE_SERIAL_UART (( BL_TYPE_STANDALONE << 8U) | 0x01U) |
Macro defining the extended standalone UART bootloader type.
| #define BL_EXT_TYPE_SERIAL_UART_OTA (( BL_TYPE_STANDALONE << 8U) | 0x03U) |
Macro defining the extended standalone OTA and UART bootloader type.
| #define BL_EXT_TYPE_SERIAL_USB (( BL_TYPE_STANDALONE << 8U) | 0x07U) |
Macro defining the extended standalone USB bootloader type.
| #define BL_EXT_TYPE_SERIAL_USB_OTA (( BL_TYPE_STANDALONE << 8U) | 0x08U) |
Macro defining the extended standalone OTA and USB bootloader type.
| #define BL_EXT_TYPE_STANDALONE_UNKNOWN (( BL_TYPE_STANDALONE << 8U) | 0x00U) |
Macro defining the extended standalone unknown bootloader type.
| #define BL_TYPE_APPLICATION (2) |
Numerical definition for a bootloader type.
| #define BL_TYPE_BOOTLOADER (3) |
Numerical definition for a bootloader type.
| #define BL_TYPE_NULL (0) |
Numerical definition for a bootloader type.
| #define BL_TYPE_SMALL_BOOTLOADER (4) |
Numerical definition for a bootloader type.
| #define BL_TYPE_STANDALONE (1) |
Numerical definition for a bootloader type.
| #define BOOTLOADER_BASE_TYPE | ( |
extendedType
|
) | ((uint8_t)(((extendedType) >> 8U) & 0xFFU)) |
Macro returning the base type of a bootloader when given an extended type.
| #define BOOTLOADER_INVALID_VERSION 0xFFFF |
Define an invalid bootloader version.
| #define BOOTLOADER_MAKE_EXTENDED_TYPE | ( |
baseType,
|
|
extendedSpecifier
|
|||
| ) | ((uint16_t)(((uint16_t)baseType) << 8U) | (((uint16_t)extendedSpecifier) & 0xFFU)) |
Macro returning the extended type of a bootloader when given a base type and extendedSpecifier.
| #define CUSTOMER_APPLICATION_CAPABILITIES 0 |
Macro defining the customer application capabilities stored in the ApplicationProperties_t struct.
- Note
- The capabilities field in the ApplicationProperties_t struct is shared with other values.
| #define CUSTOMER_APPLICATION_PRODUCT_ID { 0 } |
Macro defining the customer application product ID stored in the ApplicationProperties_t struct.
| #define CUSTOMER_APPLICATION_VERSION 0 |
Macro defining the customer application version stored in the ApplicationProperties_t struct.
| #define MPSI_PLUGIN_SUPPORT 0 |
Macro defining the support for the MPSI protocol stored in the capabilities field of the ApplicationProperties_t struct.
Typedef Documentation
| typedef uint8_t BlBaseType |
Define the bootloader base type.
| typedef uint16_t BlExtendedType |
Define the bootloader extended type.
Function Documentation
| BlExtendedType halBootloaderGetInstalledType | ( | void |
|
) |
Returns the extended bootloader type of the bootloader that is present on the chip.
| BlBaseType halBootloaderGetType | ( | void |
|
) |
Returns the bootloader base type the application was built for.
- Returns
- BL_TYPE_NULL , BL_TYPE_STANDALONE , or BL_TYPE_APPLICATION
| uint16_t halGetBootloaderVersion | ( | void |
|
) |
Returns the version of the installed bootloader, regardless of its type.
- Returns
- Version if bootloader installed, or BOOTLOADER_INVALID_VERSION . A returned version of 0x1234U would indicate version 1.2 build 34
| void halGetExtendedBootloaderVersion | ( | uint32_t * |
emberVersion,
|
| uint32_t * |
customerVersion
|
||
| ) |
Return extended bootloader version information, if supported. This API is not supported for EM2XX chips and only returns extra information on bootloaders built on or after the 4.7 release.
- Parameters
-
emberVersionIf specified, we will return the full 32bit ember version for this bootloader. Format is major, minor, patch, doc (4bit nibbles) followed by a 16bit build number. customerVersionThis will return the 32bit value specified in CUSTOMER_BOOTLOADER_VERSION at build time.