EmberZllNetwork Struct Reference
Information about the ZLL network and specific device that responded to a ZLL scan request.
#include <
zll-types.h
>
Data Fields |
|
| EmberZigbeeNetwork | zigbeeNetwork |
| EmberZllSecurityAlgorithmData | securityAlgorithm |
| EmberEUI64 | eui64 |
| EmberNodeId | nodeId |
| EmberZllState | state |
| EmberNodeType | nodeType |
| uint8_t | numberSubDevices |
| uint8_t | totalGroupIdentifiers |
| uint8_t | rssiCorrection |
Information about the ZLL network and specific device that responded to a ZLL scan request.
Field Documentation
| EmberEUI64 EmberZllNetwork::eui64 |
| EmberNodeId EmberZllNetwork::nodeId |
| EmberNodeType EmberZllNetwork::nodeType |
| uint8_t EmberZllNetwork::numberSubDevices |
| uint8_t EmberZllNetwork::rssiCorrection |
| EmberZllSecurityAlgorithmData EmberZllNetwork::securityAlgorithm |
| EmberZllState EmberZllNetwork::state |
| uint8_t EmberZllNetwork::totalGroupIdentifiers |
| EmberZigbeeNetwork EmberZllNetwork::zigbeeNetwork |
The documentation for this struct was generated from the following file:
-
zll-types.h