Binding Table
EmberZNet binding table API.
Functions |
|
| EmberStatus | emberSetBinding (uint8_t index, EmberBindingTableEntry *value) |
Sets an entry in the binding table by copying the structure pointed to by
value
into the binding table.
|
|
| EmberStatus | emberGetBinding (uint8_t index, EmberBindingTableEntry *result) |
Copies a binding table entry to the structure that the
result
points to.
|
|
| EmberStatus | emberDeleteBinding (uint8_t index) |
|
Deletes a binding table entry.
|
|
| bool | emberBindingIsActive (uint8_t index) |
|
Indicates whether any messages are currently being sent using this binding table entry.
|
|
| EmberNodeId | emberGetBindingRemoteNodeId (uint8_t index) |
|
Returns the node ID for the binding's destination if the ID is known.
|
|
| void | emberSetBindingRemoteNodeId (uint8_t index, EmberNodeId id) |
|
Sets the node ID for the binding's destination. See
emberGetBindingRemoteNodeId()
for a description.
|
|
| EmberStatus | emberClearBindingTable (void) |
|
Deletes all binding table entries.
|
|
| EmberZdoStatus | emberRemoteSetBindingHandler ( EmberBindingTableEntry *entry) |
|
A callback invoked when a remote node requests that a binding be added to the local binding table (via the ZigBee Device Object at endpoint 0).
|
|
| EmberZdoStatus | emberRemoteDeleteBindingHandler (uint8_t index) |
|
A callback invoked when a remote node requests that a binding be removed from the local binding table (via the ZigBee Device Object at endpoint 0).
|
|
| uint8_t | emberGetBindingIndex (void) |
|
Returns a binding index that matches the current incoming message, if known.
|
|
| EmberStatus | emberSetReplyBinding (uint8_t index, EmberBindingTableEntry *entry) |
|
Creates a binding table entry for the sender of a message, which can be used to send messages to that sender.
|
|
| EmberStatus | emberNoteSendersBinding (uint8_t index) |
|
Updates the routing information associated with a binding table entry for the sender of a message.
|
|
Detailed Description
EmberZNet binding table API.
See
binding-table.h
for source code.
Function Documentation
| bool emberBindingIsActive | ( | uint8_t |
index
|
) |
Indicates whether any messages are currently being sent using this binding table entry.
Note that this function does not indicate whether a binding is clear. To determine whether a binding is clear, check the EmberBindingTableEntry structure that defines the binding. The type field should have the value EMBER_UNUSED_BINDING .
- Parameters
-
indexThe index of a binding table entry.
- Returns
- True if the binding table entry is active, false otherwise.
| EmberStatus emberClearBindingTable | ( | void |
|
) |
Deletes all binding table entries.
- Returns
-
An
EmberStatusvalue that indicates the success or failure of the command.
| EmberStatus emberDeleteBinding | ( | uint8_t |
index
|
) |
Deletes a binding table entry.
- Parameters
-
indexThe index of a binding table entry.
- Returns
-
An
EmberStatusvalue that indicates the success or failure of the command.
| EmberStatus emberGetBinding | ( | uint8_t |
index,
|
| EmberBindingTableEntry * |
result
|
||
| ) |
Copies a binding table entry to the structure that the
result
points to.
- Parameters
-
indexThe index of a binding table entry. resultA pointer to the location to which to copy the binding table entry.
- Returns
-
An
EmberStatusvalue that indicates the success or failure of the command.
| uint8_t emberGetBindingIndex | ( | void |
|
) |
Returns a binding index that matches the current incoming message, if known.
A binding matches the incoming message if:
- The binding's source endpoint is the same as the message's destination endpoint.
- The binding's destination endpoint is the same as the message's source endpoint.
- The source of the message has been previously identified as the the binding's remote node by a successful address discovery or by the application via a call to either emberSetReplyBinding() or emberNoteSendersBinding() .
- Note
- This function can be called only from within emberIncomingMessageHandler() .
- Returns
-
The index of a binding that matches the current incoming message or
0xFFif there is no matching binding.
| EmberNodeId emberGetBindingRemoteNodeId | ( | uint8_t |
index
|
) |
Returns the node ID for the binding's destination if the ID is known.
If a message is sent using the binding and the destination's ID is not known, the stack will discover the ID by broadcasting a ZDO address request. The application can avoid the need for this discovery by calling emberNoteSendersBinding() whenever a message arrives from the binding's destination, or by calling emberSetBindingRemoteNodeId() when it knows the correct ID via some other means, such as having saved it in nonvolatile memory.
The destination's node ID is forgotten when the binding is changed, when the local node reboots or, much more rarely, when the destination node changes its ID in response to an ID conflict.
- Parameters
-
indexThe index of a binding table entry.
- Returns
- The short ID of the destination node or EMBER_NULL_NODE_ID if no destination is known.
| EmberStatus emberNoteSendersBinding | ( | uint8_t |
index
|
) |
Updates the routing information associated with a binding table entry for the sender of a message.
This function should be used in place of emberSetReplyBinding() when a message arrives from a remote endpoint for which a binding already exists.
- Parameters
-
indexThe index of the binding to update.
- Returns
-
An
EmberStatusvalue that indicates the success or failure of the command.
| EmberZdoStatus emberRemoteDeleteBindingHandler | ( | uint8_t |
index
|
) |
A callback invoked when a remote node requests that a binding be removed from the local binding table (via the ZigBee Device Object at endpoint 0).
The application is free to remove the binding from the binding table, ignore the request, or take some other action.
If the application includes emberRemoteDeleteBindingHandler() , it must define EMBER_APPLICATION_HAS_REMOTE_BINDING_HANDLER in its CONFIGURATION_HEADER and also include emberRemoteSetBindingHandler() .
- Parameters
-
indexThe index of the binding entry to be removed.
- Returns
- EMBER_ZDP_SUCCESS if the binding was removed from the table EMBER_ZDP_NOT_AUTHORIZED if permission was denied EMBER_ZDP_NOT_PERMITTED if the binding is active EMBER_ZDP_NO_ENTRY if the binding doesn't exist
| EmberZdoStatus emberRemoteSetBindingHandler | ( | EmberBindingTableEntry * |
entry
|
) |
A callback invoked when a remote node requests that a binding be added to the local binding table (via the ZigBee Device Object at endpoint 0).
The application is free to add the binding to the binding table, ignore the request, or take some other action. It is recommended that nonvolatile bindings be used for remote provisioning applications.
The binding's type defaults to EMBER_UNICAST_BINDING . The application should set the type as appropriate for the binding's local endpoint and cluster ID.
If the application includes emberRemoteSetBindingHandler() , it must define EMBER_APPLICATION_HAS_REMOTE_BINDING_HANDLER in its CONFIGURATION_HEADER and also include emberRemoteDeleteBindingHandler() .
- Parameters
-
entryA pointer to a new binding table entry.
- Returns
- EMBER_ZDP_SUCCESS if the binding was added to the table EMBER_ZDP_NOT_AUTHORIZED if permission was denied EMBER_ZDP_NOT_PERMITTED if the binding is active EMBER_ZDP_TABLE_FULL if there is no more space in the binding table
| EmberStatus emberSetBinding | ( | uint8_t |
index,
|
| EmberBindingTableEntry * |
value
|
||
| ) |
Sets an entry in the binding table by copying the structure pointed to by
value
into the binding table.
- Note
-
You do not need to reserve memory for
value.
- Parameters
-
indexThe index of a binding table entry. valueA pointer to a structure.
- Returns
-
An
EmberStatusvalue that indicates the success or failure of the command.
| void emberSetBindingRemoteNodeId | ( | uint8_t |
index,
|
| EmberNodeId |
id
|
||
| ) |
Sets the node ID for the binding's destination. See emberGetBindingRemoteNodeId() for a description.
- Parameters
-
indexThe index of a binding table entry. idThe ID of the binding's destination.
| EmberStatus emberSetReplyBinding | ( | uint8_t |
index,
|
| EmberBindingTableEntry * |
entry
|
||
| ) |
Creates a binding table entry for the sender of a message, which can be used to send messages to that sender.
This function is identical to emberSetBinding() except that calling it tells the stack that this binding corresponds to the sender of the current message. The stack uses this information to associate the sender's routing info with the binding table entry.
- Note
- This function may only be called from within emberIncomingMessageHandler() .
- Parameters
-
indexThe index of the binding to set. entryA pointer to data for the binding.
- Returns
-
An
EmberStatusvalue that indicates the success or failure of the command.