EmberApsFrame Struct Reference
An in-memory representation of a ZigBee APS frame of an incoming or outgoing message.
#include <
ember-types.h
>
Data Fields |
|
| uint16_t | profileId |
| uint16_t | clusterId |
| uint8_t | sourceEndpoint |
| uint8_t | destinationEndpoint |
| EmberApsOption | options |
| uint16_t | groupId |
| uint8_t | sequence |
| uint8_t | radius |
An in-memory representation of a ZigBee APS frame of an incoming or outgoing message.
Field Documentation
| uint16_t EmberApsFrame::clusterId |
The cluster ID for this message.
| uint8_t EmberApsFrame::destinationEndpoint |
The destination endpoint.
| uint16_t EmberApsFrame::groupId |
The group ID for this message, if it is multicast mode.
| EmberApsOption EmberApsFrame::options |
A bitmask of options from the enumeration above.
| uint16_t EmberApsFrame::profileId |
The application profile ID that describes the format of the message.
| uint8_t EmberApsFrame::radius |
| uint8_t EmberApsFrame::sequence |
The sequence number.
| uint8_t EmberApsFrame::sourceEndpoint |
The source endpoint.
The documentation for this struct was generated from the following file:
-
ember-types.h