Data structure of the relay event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_diagnostic_relay_s::destination_address
Message destination address
Definition at line
22364
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
source_address#
uint16_t sl_btmesh_evt_diagnostic_relay_s::source_address
Message source address
Definition at line
22365
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
rssi#
int8_t sl_btmesh_evt_diagnostic_relay_s::rssi
RSSI value of the relayed message. Units: dBm.
Definition at line
22366
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
ttl#
uint8_t sl_btmesh_evt_diagnostic_relay_s::ttl
Time-to-Live value of the relayed or proxied message
Definition at line
22368
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h