Data structure of the distribution_status event.
Public Attributes#
uint16_t
uint16_t
uint8_t
uint8_t
uint16_t
uint16_t
uint8_t
uint16_t
uint8_t
uint8_t
uint16_t
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::elem_index
Client model element index
Definition at line
18428
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::server_address
Unicast address of the server
Definition at line
18429
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::status
Enum sl_btmesh_fw_dist_server_dist_status_t. Status code returned
Definition at line
18430
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
phase#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::phase
Enum sl_btmesh_fw_dist_client_dist_phase_t. Phase of the Distribution Server
Definition at line
18433
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
group_address#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::group_address
Distribution group address. Ignore if no distribution is active.
Definition at line
18436
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::appkey_index
Distribution app key index. Ignore if no distribution is active.
Definition at line
18438
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
distributor_ttl#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::distributor_ttl
TTL used by the Distributor. Ignore if no distribution is active.
Definition at line
18440
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
timeout_base#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::timeout_base
Timeout Base value used in BLOB Transfer
Definition at line
18442
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transfer_mode#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::transfer_mode
Transfer Mode used in BLOB Transfer
Definition at line
18443
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
apply_immediately#
uint8_t sl_btmesh_evt_fw_dist_client_distribution_status_s::apply_immediately
1 if the Update Policy is Verify and Apply, otherwise 0. Ignore if no distribution is active.
Definition at line
18444
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fw_list_index#
uint16_t sl_btmesh_evt_fw_dist_client_distribution_status_s::fw_list_index
Index of the firmware in the Distributor's Firmware List
Definition at line
18447
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h