Data structure of the receivers_status event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_status_s::elem_index
Client model element index
Definition at line
18303
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_status_s::server_address
Unicast address of the server
Definition at line
18304
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_fw_dist_client_receivers_status_s::status
Enum sl_btmesh_fw_dist_server_dist_status_t. Status code returned
Definition at line
18305
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
nodes_list_size#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_status_s::nodes_list_size
Number of entries currently in the node list
Definition at line
18308
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h