Data structure of the upload_status event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_client_upload_status_s::elem_index
Client model element index
Definition at line
18469
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_fw_dist_client_upload_status_s::server_address
Unicast address of the server
Definition at line
18470
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_fw_dist_client_upload_status_s::status
Enum sl_btmesh_fw_dist_server_dist_status_t. Status code returned
Definition at line
18471
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
phase#
uint8_t sl_btmesh_evt_fw_dist_client_upload_status_s::phase
Upload Phase of the Distribution Server
Definition at line
18474
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
type#
uint8_t sl_btmesh_evt_fw_dist_client_upload_status_s::type
Enum sl_btmesh_fw_dist_client_dist_upload_type_t. Upload Type of an upload (0:in-band 1:out-of-band). Ignore if no upload is active.
Definition at line
18475
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
progress#
uint8_t sl_btmesh_evt_fw_dist_client_upload_status_s::progress
0-100, percentage of BLOB Transfer octets or out-of-band data delivered and confirmed. Ignore if no upload is active.
Definition at line
18479
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fwid#
uint8array sl_btmesh_evt_fw_dist_client_upload_status_s::fwid
FWID of the firmware being transferred. Empty if no upload is active.
Definition at line
18482
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h