Data structure of the info_status_update_uri event.

Public Attributes#

uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_update_client_info_status_update_uri_s::elem_index

Client model element index


Definition at line 13111 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_fw_update_client_info_status_update_uri_s::server_address

Unicast address of the server


Definition at line 13112 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

index#

uint8_t sl_btmesh_evt_fw_update_client_info_status_update_uri_s::index

Index of this URI in the Firmware Information List


Definition at line 13113 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

count#

uint8_t sl_btmesh_evt_fw_update_client_info_status_update_uri_s::count

Total number of entries in the Firmware Information List


Definition at line 13115 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

update_uri#

uint8array sl_btmesh_evt_fw_update_client_info_status_update_uri_s::update_uri

Update URI


Definition at line 13117 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h