Data structure of the server_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_health_client_server_status_s::client_address

Destination address the message was sent to


Definition at line 4531 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_health_client_server_status_s::elem_index

Client model element index. Identifies the client model which received the status message.


Definition at line 4532 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_health_client_server_status_s::server_address

Address of the Server model which sent the message


Definition at line 4535 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

result#

uint16_t sl_btmesh_evt_health_client_server_status_s::result

Response status. If an error occurs (e.g., request timeout), the parameters other than element index, client address, and server address are to be ignored.


Definition at line 4537 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

current#

uint8_t sl_btmesh_evt_health_client_server_status_s::current

Whether the event lists current fault array or registered fault array


Definition at line 4541 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

test_id#

uint8_t sl_btmesh_evt_health_client_server_status_s::test_id

Test ID


Definition at line 4543 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

vendor_id#

uint16_t sl_btmesh_evt_health_client_server_status_s::vendor_id

Bluetooth vendor ID used in the request


Definition at line 4544 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

faults#

uint8array sl_btmesh_evt_health_client_server_status_s::faults

Fault array. See the Bluetooth Mesh Profile specification for a list of defined fault IDs.


Definition at line 4545 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h