Data structure of the attention event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_health_server_attention_s::elem_index
Index of the element for which attention timer was set
Definition at line
4886
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
timer_sec#
uint8_t sl_btmesh_evt_health_server_attention_s::timer_sec
Timer value in seconds. If zero, user attention is no longer required.
Definition at line
4888
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h