Data structure of the set_property event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::destination_address
Address of the server or the group address to which it was published.
Definition at line
14390
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::elem_index
Index of the element which received the command.
Definition at line
14392
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::client_address
Device which sent the request.
Definition at line
14394
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::appkey_index
Appkey used by client_address.
Definition at line
14395
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
property_id#
uint16_t sl_btmesh_evt_lc_setup_server_set_property_s::property_id
Property ID
Definition at line
14396
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
property_value#
uint8array sl_btmesh_evt_lc_setup_server_set_property_s::property_value
Property value
Definition at line
14397
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h