Data structure of the query_block_status_complete event.

Public Attributes#

uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_mbt_client_query_block_status_complete_s::elem_index

The client model element index.


Definition at line 10550 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

block_complete#

uint8_t sl_btmesh_evt_mbt_client_query_block_status_complete_s::block_complete

Non-zero if the block is complete.


Definition at line 10551 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transfer_complete#

uint8_t sl_btmesh_evt_mbt_client_query_block_status_complete_s::transfer_complete

Non-zero if the transfer is complete.


Definition at line 10552 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h