Data structure of the send_chunk_request event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_client_send_chunk_request_s::elem_index
The client model element index.
Definition at line
10451
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
offset#
uint32_t sl_btmesh_evt_mbt_client_send_chunk_request_s::offset
The chunk offset from the beginning of the BLOB.
Definition at line
10452
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
length#
uint16_t sl_btmesh_evt_mbt_client_send_chunk_request_s::length
The number of bytes requested.
Definition at line
10453
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h