You are viewing documentation for version:
Data structure of the server_failed event. 
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_client_server_failed_s::elem_index
The client model element index. 
server_address#
uint16_t sl_btmesh_evt_mbt_client_server_failed_s::server_address
The MBT Server address. 
timeout#
uint8_t sl_btmesh_evt_mbt_client_server_failed_s::timeout
Non-zero if a timeout occurred. 
error#
uint8_t sl_btmesh_evt_mbt_client_server_failed_s::error
Non-zero if an error occurred.