Data structure of the block_complete event.

Public Attributes#

uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_mbt_server_block_complete_s::elem_index

The server model element index.


Definition at line 11364 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_mbt_server_block_complete_s::client_address

The address of the MBT Client.


Definition at line 11365 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

blob_id#

sl_bt_uuid_64_t sl_btmesh_evt_mbt_server_block_complete_s::blob_id

The ID of the BLOB.


Definition at line 11366 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

block_number#

uint16_t sl_btmesh_evt_mbt_server_block_complete_s::block_number

The index number of the completed block.


Definition at line 11367 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

block_size#

uint16_t sl_btmesh_evt_mbt_server_block_complete_s::block_size

The size of the completed block.


Definition at line 11368 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h