Data structure of the block_start event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_server_block_start_s::elem_index
The server model element index.
Definition at line
11301
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_mbt_server_block_start_s::client_address
The address of the MBT Client.
Definition at line
11302
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_mbt_server_block_start_s::blob_id
The ID of the BLOB.
Definition at line
11303
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
block_number#
uint16_t sl_btmesh_evt_mbt_server_block_start_s::block_number
The index number of the new block.
Definition at line
11304
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
chunk_size#
uint16_t sl_btmesh_evt_mbt_server_block_start_s::chunk_size
The new block is divided into chunks of this size.
Definition at line
11305
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
block_size#
uint16_t sl_btmesh_evt_mbt_server_block_start_s::block_size
The size of the new block.
Definition at line
11307
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h