Data structure of the scan_capabilities event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
19165
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server#
uint16_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::server
Server address.
Definition at line
19166
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
max_items#
uint8_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::max_items
The maximum number of UUIDs that can be reported during scanning.
Definition at line
19167
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
active#
uint8_t sl_btmesh_evt_remote_provisioning_client_scan_capabilities_s::active
Indication if active scan is supported.
Definition at line
19169
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h