Data structure of the scan_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 19190 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server#

uint16_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::server

Server address.


Definition at line 19191 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::status

Enum sl_btmesh_remote_provisioning_server_status_t. server status.


Definition at line 19192 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

state#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::state

Enum sl_btmesh_remote_provisioning_server_scan_state_t. Scan state.


Definition at line 19195 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

max_reports#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::max_reports

Maximum number of scanned items to be reported.


Definition at line 19198 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

timeout_sec#

uint8_t sl_btmesh_evt_remote_provisioning_client_scan_status_s::timeout_sec

Maximum available time for time left until the end of the Remote Provisioning Scan procedure.


Definition at line 19199 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h