Data structure of the register_status event.

Public Attributes#

uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

destination_address#

uint16_t sl_btmesh_evt_scene_client_register_status_s::destination_address

Address of the client or the group address to which it was published.


Definition at line 14507 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_scene_client_register_status_s::elem_index

Index of the element for which received the status.


Definition at line 14509 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_scene_client_register_status_s::server_address

Device which sent the status.


Definition at line 14511 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_scene_client_register_status_s::appkey_index

Appkey used by client_address.


Definition at line 14512 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_scene_client_register_status_s::status

Status of the request.


Definition at line 14513 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

current_scene#

uint16_t sl_btmesh_evt_scene_client_register_status_s::current_scene

Currently selected scene.


Definition at line 14514 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

scenes#

uint8array sl_btmesh_evt_scene_client_register_status_s::scenes

List of stored scenes on the server derived from the Scene Register. It contains a variable length array of 16-bit values representing Scene Numbers in little endian format.


Definition at line 14515 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h