Data structure of the tx_status event.

Public Attributes#

uint16_t
uint8_t
uint8_t

Public Attribute Documentation#

server#

uint16_t sl_btmesh_evt_silabs_config_client_tx_status_s::server

Server address.


Definition at line 3812 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

status#

uint8_t sl_btmesh_evt_silabs_config_client_tx_status_s::status

Enum sl_btmesh_silabs_config_client_status_t. Status code from the Server.


Definition at line 3813 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

tx_phy#

uint8_t sl_btmesh_evt_silabs_config_client_tx_status_s::tx_phy

TX PHY for long packets (packets that would be segmented).

  • 1: LE 1M PHY

  • 2: LE 2M PHY


Definition at line 3816 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

tx_options_bitmap#

uint32_t sl_btmesh_evt_silabs_config_client_tx_status_s::tx_options_bitmap

TX options. NOTE: Currently not used: reserved for future use.


Definition at line 3820 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h