Data structure of the replay_protection_list_saved event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_test_replay_protection_list_saved_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
6356
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
saved_count#
uint16_t sl_btmesh_evt_test_replay_protection_list_saved_s::saved_count
Number of entries saved successfully
Definition at line
6357
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
total_count#
uint16_t sl_btmesh_evt_test_replay_protection_list_saved_s::total_count
Number of entries in the list in total
Definition at line
6358
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h