Data structure of the tai_utc_delta_updated event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_time_server_tai_utc_delta_updated_s::elem_index
Server model element index
Definition at line
16218
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
tai_utc_delta_current#
int32_t sl_btmesh_evt_time_server_tai_utc_delta_updated_s::tai_utc_delta_current
Current difference between TAI and UTC is seconds. Range is -255 to 32512.
Definition at line
16219
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
tai_utc_delta_new#
int32_t sl_btmesh_evt_time_server_tai_utc_delta_updated_s::tai_utc_delta_new
Upcoming difference between TAI and UTC is seconds. Range is -255 to 32512.
Definition at line
16221
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
tai_of_delta_change#
uint64_t sl_btmesh_evt_time_server_tai_utc_delta_updated_s::tai_of_delta_change
TAI Seconds time of the upcoming TAI-UTC Delta change
Definition at line
16223
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h