Data structure of the receive event.
Public Attributes#
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_vendor_model_receive_s::destination_address
Address the message was sent to. It can be either the model element's unicast address or a subscription address of the model
4126
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_vendor_model_receive_s::elem_index
Receiving model element index
4130
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
vendor_id#
uint16_t sl_btmesh_evt_vendor_model_receive_s::vendor_id
Vendor ID of the receiving model
4131
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
model_id#
uint16_t sl_btmesh_evt_vendor_model_receive_s::model_id
Model ID of the receiving model
4132
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
source_address#
uint16_t sl_btmesh_evt_vendor_model_receive_s::source_address
Unicast address of the model which sent the message
4133
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
va_index#
int8_t sl_btmesh_evt_vendor_model_receive_s::va_index
Index of the destination Label UUID (valid only is the destination address is a virtual addres)
4135
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_vendor_model_receive_s::appkey_index
The application key index used
4138
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
nonrelayed#
uint8_t sl_btmesh_evt_vendor_model_receive_s::nonrelayed
If non-zero, indicates that the received message was not relayed (TTL was zero), which means that the devices are within direct radio range of each other.
4139
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
message_flags#
uint8_t sl_btmesh_evt_vendor_model_receive_s::message_flags
Unsigned 8-bit integer
4143
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
opcode#
uint8_t sl_btmesh_evt_vendor_model_receive_s::opcode
Message opcode
4144
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
final#
uint8_t sl_btmesh_evt_vendor_model_receive_s::final
Indicates whether this payload chunk is the final one of the message or whether more will follow
4145
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
payload#
uint8array sl_btmesh_evt_vendor_model_receive_s::payload
Payload data (either complete or partial; see final parameter)
4148
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h