Data structure of the send_complete event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_vendor_model_send_complete_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
4178
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint16_t sl_btmesh_evt_vendor_model_send_complete_s::handle
Tracking handle for the message sending attempt as reported by sl_btmesh_vendor_model_send_tracked or sl_btmesh_vendor_model_set_publication_tracked command responses.
Definition at line
4179
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
message_flags#
uint8_t sl_btmesh_evt_vendor_model_send_complete_s::message_flags
Unsigned 8-bit integer
Definition at line
4184
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h