sl_btmesh_evt_mbt_client_send_chunks_complete#

All chunks in the current block have been sent.

Each block is transferred in chunks, sending the chunks to the servers which have them missing. This event indicates that a single round of sending those chunks is complete.

After receiving this event, the block status should be queried from the servers with the sl_btmesh_mbt_client_query_block_status command.

Modules#

sl_btmesh_evt_mbt_client_send_chunks_complete_s

Macros#

#define

Identifier of the send_chunks_complete event.

Typedef Documentation#

sl_btmesh_evt_mbt_client_send_chunks_complete_t#

typedef struct sl_btmesh_evt_mbt_client_send_chunks_complete_s sl_btmesh_evt_mbt_client_send_chunks_complete_t

Definition at line 10597 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_mbt_client_send_chunks_complete_id#

#define sl_btmesh_evt_mbt_client_send_chunks_complete_id
Value:
0x082800a8

Identifier of the send_chunks_complete event.


Definition at line 10587 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h